This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F6779A: Does the SYS16 errata cause the device temporarily reset only (not hold reset)?

Part Number: MSP430F6779A


Does the SYS16 errata cause the device temporarily reset only (not hold reset)?

  • See from the descirption, I think it is yes. Here is the comment I find in the system:

    2. What is the noticeable effect for a customer or what is the applicative/functional malfunction caused by this bug: 
    
    Could issue a false reset (as long as 60uS) even when supply is good but has an up transient as low as 300mV  (could be lower  with multiple transients).
    

**Attention** This is a public forum