This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5308: Rev F devices MCLK can not stable under 24MHz

Part Number: MSP430F5308

Is the UCS system in RevF material different from that of Rev C or Rev D devices? 

I tried using an external oscillator to provide a 24MHz clock signal and could not get MCLK stable with OFIFG remaining "one". It can only work under clock frequency around 21MHz or below, while Rev C and Rev D material did show this signature. I used internal Refclk generated through FLL to generate a 24MHz signal and get the same result. Can anyone help to clarify?

**Attention** This is a public forum