Part Number: MSP430FR5994
Hello,
I recently resumed work with a MSP430FR5994 project that was successfully built with V8.2 of CCS in 2018. I installed the current version of CCS (V12.6) and the application builds fine and runs,
However, the previously functioning chip temperature calculation no longer work correctly, because the pointers to:
#define CALADC12_12V_30C *( (unsigned int *) 0x1A1A ) // Temperature Sensor Calibration-30 C
// See device datasheet for TLV table memory mapping
#define CALADC12_12V_85C *( (unsigned int *) 0x1A1C ) // Temperature Sensor Calibration-85 C
no longer work. This morning I run the original loaded test program and it still worked fine. After rebuilding it in V12.6 it failed the temperature calculation due to incorrect data retrieved at the specified address.
Is there a work around or fix to access the referenced calibration constants?
Please let me know if this is an isolated problem or a common issue and if there is a work around. I will try tonight to find my old installation and test it again with V8.2 of the CCS.
Regards,
Gerhard