Hi! I'm using the EVM430-FR6043 to measure water flow.
It measures well in USS
So I created header file using USS( Design Center)
and copied it into the "USSSWLib_template_example" Project
When I ran it, I only got zero values.
Like this:
$,00000000
#,00000000
I'm curious to verify if the measurements are accurate, so I want to check the capture data
Where can I find the ultrasound capture data in 'USSSWLib_template_example'?