I am planning to use MSP430FR2475TRHB
The datasheet SLASEO7C – MARCH 2019 – REVISED SEPTEMBER 2021 states on page 55 :
'The CCR0 registers on both TA0 and TA2 are not
externally connected and can only be used for hardware period timing and interrupt generation'
but on Page 60 Fig 9-3 TA2 graphics shows CCR0 TA2.OA connected to P2.3, this is also repeated in Table 9-14.
Which is correct?
Can I use this output to generate a clock signal to another peripheral.