This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2476: MSP430FR2476_Clock settings

Part Number: MSP430FR2476


ACLK ~32kHz, DCO=MCLK = SMCLK = 4MHz
What would the code look like if I wanted to configure it as above?
There were some parts in the sample code that were difficult to understand.
I would appreciate it if you could provide me with the code and a brief explanation regarding the settings.
Also, what is the setting for "REFO"?
I'm sorry that I didn't have time and asked the question before I looked into it in depth.
Thank you.

**Attention** This is a public forum