Part Number: MSP430FR50431
Hi,
Following our conversations -
Today we burned the template code of 6047 on our card that contains the msp50431, we changed the target in the build setting so that the cmd file changed for 50431.
In this case we got a good ADC, and correct water readings.
When we burned the template code of 6043 on our card that contains the msp50431 we changed the target in the build setting so that the cmd file changed for 50431.
In this case we got a bad ADC and correspondingly bad water readings.
Why is this happening?
Could it be that the template code of 6043 is set to gas and therefore the ADC is not good?
I note that this is a clean file from your website, and I only entered that they both have USS_config.h
so that there are no differences in the configuration.