Part Number: MSP430FR6047
I received the EVM430-FR6037 board and proceeded to hook it up to 1MHz sensors and found that the device worked wonderfully using the USS Software. However, I have since loaded in some example programs into the device so that I could change the frequency of the pulse. This is due to the software not allowing me to go below the 780kHz. This too was a success. Not with the software but by loading in example code, adjusting, and monitoring with my scope. Not that I am here, I am stuck.
1. Can you send me the source files that come on the IC originally? Now that I see that it works, I want to be able to go back. The website has plenty of example codes, but I cannot tell which one, if any, is the original.
2. Can you assist me in changing your software to allow me to send 250kHz pulses?
Best Regards,
Matt L.