Part Number: MSP430G2231
I attempted to create a small clock using a MAX7219 for the display. I wrote some code, and while the display does show, it gets stuck at the end. During debugging, I noticed that when I pause the program, it stops on the following line:
while (!(USICTL1 & USIIFG));
I implemented a quick fix by limiting the cycles with an escape counter.
Is there an error in my configuration?
#include <msp430.h>
#include "msp430g2231.h"
#include <stdint.h>
#include <stdbool.h>
#include "max7219.h"
void SetSPI(void);
void SetI2C(void);
#define MODE_SPI 0x00
#define MODE_I2C 0x01
#define BUSY_SPI 0x02
#define BUSY_I2C 0x04
#define REQ_SPI 0x08
#define REQ_I2C 0x10
void changeUSI(int modo) {
// Deshabilitar el USI
USICTL0 |= USISWRST;
if (modo == MODE_SPI) {
SetSPI();
} else if (modo == MODE_I2C) {
SetI2C();
}
// Habilitar el USI
USICTL0 &= ~USISWRST;
}
void SetSPI(void){
USICTL0 = USIPE6 + USIPE5 + USIMST + USIOE;
USICTL1 = USICKPH;
USICKCTL |= USIDIV_0 + USISSEL_2;
USICNT = USI16B;
}
void SetI2C(void){
USICTL0 = USIPE6 + USIPE5 + USIMST + USIOE;
USICTL1 |= USICKPH;
USICKCTL |= USIDIV_0 + USISSEL_2;
}
void enviar(uint8_t comando, uint8_t dato) {
// Cargar el byte en el registro USISR
USISRH = comando;
USISRL = dato;
int scape = 10;
P1OUT &= ~BIT4;
USICNT |= 16;
// Limpiar la bandera de interrupción de contador USI
USICTL1 &= ~USIIFG;
// Esperar a que se complete la transmisión
while (!(USICTL1 & USIIFG) && --scape);
P1OUT |= BIT4; // Establecer P1.4 en alto después de la transmisión
}
int main(void) {
WDTCTL = WDT_ADLY_250; // WDT 250ms, ACLK, interval timer
IE1 |= WDTIE; // Enable WDT interrupt
if (CALBC1_1MHZ == 0xFF) // If calibration constants erased
{
while (1)
; // do not load, trap CPU!!
}
DCOCTL = 0; // Select lowest DCOx and MODx settings
BCSCTL1 = CALBC1_1MHZ;
DCOCTL = CALDCO_1MHZ;
BCSCTL3 |= XCAP_3; //LFXTAL Capacitor 12.5pf
P1OUT = BIT4 | BIT3 | BIT7; // Initialize all GPIO
P1SEL = UART_TXD + UART_RXD; // Timer function for TXD/RXD pins
P1DIR = 0xFF & ~(UART_RXD | BIT7 | BIT3); // Set all pins but RXD to output
P1REN = BIT3 | BIT7;
P2OUT = 0x00;
//P2SEL = 0x00;
P2DIR = 0x3F;
__enable_interrupt();
TimerA_UART_init(); // Start Timer_A UART
TimerA_UART_print("G2xx1 TimerA UART\r\n");
TimerA_UART_print("READY.\r\n");
uint8_t bitcount = 1;
TimerA_UART_print("Config Module 1\r\n");
TimerA_UART_print("Set SPI\r\n");
changeUSI(MODE_SPI);
TimerA_UART_print("Shutdown\r\n");
enviar(SHUTDOWN, SHUTDOWN_MODE);
TimerA_UART_print("Display Limit\r\n");
enviar(SCAN_LIMIT, DISPLAY_7);
TimerA_UART_print("Intensity\r\n");
enviar(INTENSITY, DUTY_CYCLE_15_32);
TimerA_UART_print("Decode Mode\r\n");
enviar(DECODE_MODE, 0xFF);
TimerA_UART_print("Test Off\r\n");
enviar(DISPLAY_TEST, TEST_NORMAL_OPERATION);
TimerA_UART_print("Turn On\r\n");
enviar(SHUTDOWN, SHUTDOWN_NORMAL_OPERATION);
TimerA_UART_print("Digits\r\n");
enviar(DIGIT_0, 1);
enviar(DIGIT_1, 2);
enviar(DIGIT_2, 3);
enviar(DIGIT_3, 4);
enviar(DIGIT_4, 5);
enviar(DIGIT_5, 6);
enviar(DIGIT_6, 7);
enviar(DIGIT_7, 8);
enviar(0,0);
for (;;) {
// Wait for incoming character
__bis_SR_register(LPM0_bits);
TimeReport();
// Echo received character
//TimerA_UART_tx(rxBuffer);
}
}