Part Number: MSP430FR2433
Hey all, just wanted to share a library that makes it easy to use threads with MSP430 chips:
https://github.com/toasterllc/Scheduler
It's a single header so it's easy to integrate.
Below is a two-thread example: the first thread toggles an LED every second, the second thread waits for a button to be pressed and then rapidly toggles a second LED.
Cheers,
David
void TaskLED::Run() {
for (;;) {
P1OUT ^= BIT0;
Scheduler::Sleep(Scheduler::Ms<1000>);
}
}
void TaskButton::Run() {
for (;;) {
Scheduler::Wait([] { return _Pressed; });
for (int i=0; i<100; i++) {
P1OUT ^= BIT1;
Scheduler::Sleep(Scheduler::Ms<20>);
}
_Pressed = false;
}
}