Part Number: MSP430FG6626
Other Parts Discussed in Thread: MSP-FET,
Hi everybody ,
I am using MSP430FG6626 in eval board MSP-TS430PZ100AUSB + emulator TI MSP-FET, Code Composer 12.7.0.00007
I m testing example cstd16_ex2_singleChSingleConvPolling project : I can compile , download debug etc
now issue is : I only see random values in RESULTS variable ( I m following instruction in the code example ) : I can apply on Vin* and - both "0" V or "0.3" I only get random results ( they change everytime I rerun the example )
where am I wrong ? what shoudl I do ?
FYI the evm as is you measure on Vref about 0.5V --- is it correct ? shuould I apply a different Voltage to Vref and how ?
any suggestion or another exaple to test is very welcome
thank you
BR
Carlo