Part Number: MSP-FET
Other Parts Discussed in Thread: ENERGIA, UNIFLASH, CCSTUDIO, , RF430FRL152HEVM, TRF7970A, RF430FRL152H, MSP-EXP430G2ET
Hi,
I was using the MSP-FET tool to update the firmware of RF430FRL152HEVM with the JTAG interface. When I started updating the firmware a message 'error recognizing the MSP-FET tool' popped up in the CCStudio IDE. I clicked on Recover option at the IDE prompt and shortly after that I received the message 'error recognizing ez-FET tool, only one FET tool should be connected at one time'. I checked under Device manager and my system is not able to recognize the MSP-FET tool now. I tried the solutions discussed on the forums related to this topic but I am not able to resolve the issue still. When I power up the RF430FRL152HEVM using USB cable both the alarm and power LEDs turn on. Does that mean the EVM is not working? I tried updating the firmware using 3 different systems but I am getting the same message on all 3 systems. I even tried using Energia and UniFlash to update the firmware but the issue wasn't resolved. Is the MSP-FET tool completely bricked? Do I need to purchase a new MSP-FET tool or RF430FRL152HEVM? I need to update the firmware ASAP to move onto the next stage of development of the project. Any help in resolving the issue is greatly appreciated.