Other Parts Discussed in Thread: MSP430FR2433, MSP-FET, ENERGIA
Tool/software: Code Composer Studio
Hi,
I just received the TI launchpad for the MSP430FR2433 and wanted to try an example program. So I booted up CCS and loaded the 'Hello World' program for the proper MCU, which should print Hello World on a preferred output. I assumed this was over the USB UART so I opened Docklight (prefered console program), found the MSP UART Application port, opened a connection, and flashed the hello world program.
Here's where the problem started:
CCS asked me to update the firmware of the launchpad before flashing by pressing OK or Continue in a dialogue box.
The firmware flash failed and the USB devices (1 for UART application and 1 other standard device of the launchpad) in Windows device manager are gone.
Afterwards CCS said :
"MSP430: Error initializing emulator: One of the connected MSP-FETs / eZ-FETs debuggers needs recovery. Select 'Recover' to start the recovery process. Note: Only one MSP-FET / eZ-FET debugger can be connected to your system during recovery."
So I did, but it gave the error
"MSP430: Error: MSP-FET / eZ-FET recovery failed".
I updated CCS to the most recent version through CCS itself and tried recovering, to no avail.
I think the brick happened because I had an open connection with the USB UART with 3rd party software while the firmware update was running.
I found some issues like this on the forums but they're all closed because the user didn't respond on the forum thread anymore. Is there a way to solve this issue?
With kind regards,
Merijn