Tool/software:
Hello,
I have a Problem in the CCS device MSP430FR6047. I was able to run the example "C:\ti\msp\UltrasonicWaterFR604x_02_40_00_00\examples\USS_Water_Demo" without problem.
After i created an Empty Project and i wanted to import only the functions and library i needed. Communicationsfolder works without problem. But i have a problem in ussSwLib.h every function in this file can not be found from other files in the Project. i get an error "unresolved symbol " every time the function in this file is called. the problem is, i can not find, in which folder or file the function are programmed. this may be the problem.
can some one give me a hint, of which file i'm missing? i have attached a picture of the Include paths and projects folder. i tried to compare my project with that one from example, the look the same. so i don't know what is wrong. and when i comment every function from ussSwLib.h (when called) the sw runs without problem.
this is an example of the error i get:
Description Resource Path Location Type
unresolved symbol USS_runAlgorithmsFixedPoint, first referenced in ./USSLibGUIApp/fr6047_USS_app/USSLibGUIApp.obj FM44SWPLATINE4_1 C/C++ Problem
thank you
Pierre