Tool/software:
Hi, The following is two signal using the same circuit and transducer with the Number of Pulses set to 8(left) and 16(right).
Of course the Gain Control is little different.
I will be using this system in a noisy environment.
How do I set it up so that it's close to the standard for signal processing(1) and meet fewer errors?(2)