MSP430FG437: With a power source integrating a lithium ion battery and amorphous silicon solar module

Part Number: MSP430FG437

Tool/software:

Hi Experts,

Good day!

A pulse oximeter based on a Texas Instruments MSP430 microcontroller was used for the oximeter data acquisition and processing. A photoplethysmogram (PPG) signal was acquired from a volunteer’s index finger using red (632 nm) and infrared (940 nm) light-emitting diodes (LEDs) and a silicon photodiode (PD) at 1 kHz. The PD current signal was then filtered, amplified and converted to a voltage signal. A 10-bit analog to digital converter (ADC) was used to digitize the analog signal. Finally, universal asynchronous receiver/transmitter (UART) protocol was used to send the processed data to a computer for visualization. The optoelectronic probe, LED driver, PD read circuit and microcontroller board were powered using a flexible battery.

Can you tell me what model it is and how it integrates with the OPV? srep26122.pdf 

Thank you in advance.

Best regards,

Jonathan

**Attention** This is a public forum