Tool/software:
Hi Experts,
Good day!
A pulse oximeter based on a Texas Instruments MSP430 microcontroller was used for the oximeter data acquisition and processing. A photoplethysmogram (PPG) signal was acquired from a volunteer’s index finger using red (632 nm) and infrared (940 nm) light-emitting diodes (LEDs) and a silicon photodiode (PD) at 1 kHz. The PD current signal was then filtered, amplified and converted to a voltage signal. A 10-bit analog to digital converter (ADC) was used to digitize the analog signal. Finally, universal asynchronous receiver/transmitter (UART) protocol was used to send the processed data to a computer for visualization. The optoelectronic probe, LED driver, PD read circuit and microcontroller board were powered using a flexible battery.
Can you tell me what model it is and how it integrates with the OPV? srep26122.pdf
Thank you in advance.
Best regards,
Jonathan