MSP430F5529: MSP430F5529LP: How can I variables between two isolated programs and send them to the PC via UART

Part Number: MSP430F5529
Other Parts Discussed in Thread: MSP-FET

Tool/software:

Hi Team,

While researching security isolation on MSP430F5529LP, I ran into the following issues:

I divided the overall memory area of MSP430F5529 into two parts: TCM and untrusted APP. Now I need to call the hook function in the APP to send the data in TCM RAM to the PC through UART. When I compiled the TCM and APP together into a whole file and burned it to the board for execution, the send function worked normally. However, when I first burned TCM to the board with CCS, and then called the security update function written by myself from TCM to send the APP from PC to the board for deployment through UART, and called the hook function in the APP to use the send function in TCM, the PC side did not receive any data.

What I want to ask is whether the MSP430f5529LP in my research environment can share variables between two isolated programs and can normally send shared variables after isolation?

Best Regards,

Li

**Attention** This is a public forum