Tool/software:
Hello; I try to make the FR6043 running at 16MHz.
I have downloaded the example "cs_ex2_DCO16MHz". By reading the code, I assume that the 16MHz will output from pin P3.4. But when I probed it, there is nothing coming out from this pin.
Also; I have to comment out the wait insertion line (yellow highlighted line below), otherwise it will show an error message like this.

Thanks!
Wen Li
#include "driverlib.h"
uint32_t clockValue;
void main(void)
{
//Stop WDT
WDT_A_hold(WDT_A_BASE);
//Set DCO frequency to 16MHz
CS_setDCOFreq(CS_DCORSEL_1, CS_DCOFSEL_4);
CS_initClockSignal(CS_SMCLK,CS_DCOCLK_SELECT,CS_CLOCK_DIVIDER_1);
CS_initClockSignal(CS_MCLK,CS_DCOCLK_SELECT,CS_CLOCK_DIVIDER_1);
//Set wait state to 1
//FRAMCtl_configureWaitStateControl(FRAMCTL_ACCESS_TIME_CYCLES_1);
//Set P2.0 as Output Low (for setup as ACLK).
/*
* Select Port 2
* Set Pin 0 to output Low.
*/
GPIO_setOutputLowOnPin(
GPIO_PORT_P3,
GPIO_PIN4
);
//Set P2.0 as Ternary Module Function Output.
/*
* Select Port 2
* Set Pin 0 to output Ternary Module Function, (ACLK).
*/
GPIO_setAsPeripheralModuleFunctionOutputPin(
GPIO_PORT_P3,
GPIO_PIN4,
GPIO_TERNARY_MODULE_FUNCTION
);
/*
* Disable the GPIO power-on default high-impedance mode to activate
* previously configured port settings
*/
PMM_unlockLPM5();
while(1);
}