Tool/software:
As the title says, the actual test, found that the voltage, current, power data accuracy is very high, the error is very small; However, the error of the electric energy data is very large, more than 1%. Is the electric energy not the integration of power against time? Why is the power accuracy very high, but the electric energy error is large?Sometimes the power error is very large, but the electric energy error is very small;Please refer to the following table data