This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F6779A: Application hanging when 24 Bit sigma delta ADC interrupt used || Bootloader

Part Number: MSP430F6779A

Tool/software:

Hi I am trying to make a bootloader compatible application my bootloader and application is working fine untill I enable 24 bit sigma delta interrupts in my code once i enable interrupts it get's into a hang state so can't make out what is happening. I am sharing my linker script and vector table file code.

following is in my linker script 

/******************************************************************************/
/* LINKER COMMAND FILE FOR MSPBoot BOOTLOADER USING MSP430F6779A  */
/* File generated with MSPBootLinkerGen.pl on 07-01-2024 */
/*----------------------------------------------------------------------------*/


/****************************************************************************/
/* SPECIFY THE SYSTEM MEMORY MAP                                            */
/****************************************************************************/
/* The following definitions can be changed to customize the memory map for a different device
 *   or other adjustments
 *  Note that the changes should match the definitions used in MEMORY and SECTIONS
 *
 */
/* RAM Memory Addresses */
__RAM_Start = 0x1C00;                 /* RAM Start */
__RAM_End = 0x9BFF;                     /* RAM End */
    /* RAM shared between App and Bootloader, must be reserved */
    PassWd = 0x1C00;                 /* Password sent by App to force boot  mode */
    StatCtrl = 0x1C02;             /* Status and Control  byte used by Comm */
    CI_State_Machine = 0x1C03;         /*  State machine variable used by Comm */
    CI_Callback_ptr = 0x1C04;   /* Pointer to Comm callback structure */
    /* Unreserved RAM used for Bootloader or App purposes */
    _NonReserved_RAM_Start = 0x1C08; /* Non-reserved RAM */

/* Flash memory addresses */
/* App area     : C000-E7FF & 10000-4CBFB*/
/* Download area: 4CBFC-8BFF7*/
/* Boot area    : E800-FFFF*/

__Flash_Start = 0xC000;             /* Start of Application area */
   /* Reserved Flash locations for Bootloader Area */
    __Boot_Start = 0xE800;         /* Boot flash */
    __Boot_Reset = 0xFFFE;                          /* Boot reset vector */
    __Boot_VectorTable = 0xFF80;      /* Boot vector table */
    __Boot_SharedCallbacks_Len = 6; /* Length of shared callbacks (2 calls =4B(msp430) or 8B(msp430x) */
    __Boot_SharedCallbacks = 0xFF7A; /* Start of Shared callbacks */
     _BOOT_APPVECTOR = __Boot_SharedCallbacks;       /* Definition for application table             */
    _Appl_Proxy_Vector_Start = 0xE702; /* Proxy interrupt table */
    /* Reserved Flash locations for Application Area */
 
/* MEMORY definition, adjust based on definitions above */
MEMORY
{
    SFR                     : origin = 0x0000, length = 0x0010
    PERIPHERALS_8BIT        : origin = 0x0010, length = 0x00F0
    PERIPHERALS_16BIT       : origin = 0x0100, length = 0x0100
    // RAM from _NonReserved_RAM_Start - __RAM_End
    RAM                     : origin = 0x1C08, length = 0x7FF8
	// Info Mem Sections
	INFOA                   : origin = 0x1980, length = 0x80
    INFOB                   : origin = 0x1900, length = 0x80
    INFOC                   : origin = 0x1880, length = 0x80
    INFOD                   : origin = 0x1800, length = 0x80
    // Flash from _App_Start -> (APP_PROXY_VECTORS-1)
    FLASH                   : origin = 0xC002, length = 0x2700
    FLASH2                  : origin = 0x10000, length = 0x3CBFC
    // Interrupt Proxy table from  _App_Proxy_Vector_Start->(RESET-1)
    APP_PROXY_VECTORS       : origin = 0xE702, length = 252
    // App reset from _App_Reset_Vector
    RESET                   : origin = 0xE7FE, length = 0x0002
}

/****************************************************************************/
/* SPECIFY THE SECTIONS ALLOCATION INTO MEMORY                              */
/****************************************************************************/

SECTIONS
{
    .bss        : {} > RAM                /* GLOBAL & STATIC VARS              */
    .data       : {} > RAM                /* GLOBAL & STATIC VARS              */
    .sysmem     : {} > RAM                /* DYNAMIC MEMORY ALLOCATION AREA    */
    .stack      : {} > RAM (HIGH)         /* SOFTWARE SYSTEM STACK             */

    .text:_isr  : {}  > FLASH            /* Code ISRs                         */
    #ifndef __LARGE_CODE_MODEL__
        .text       : {} >> FLASH               /* CODE                 */
    #else 
        .text       : {} >> FLASH | FLASH2      /* CODE                 */
    #endif 

        .cinit      : {} > FLASH | FLASH2        /* INITIALIZATION TABLES*/
    #ifndef __LARGE_DATA_MODEL__ 
        .const      : {} >> FLASH       /* CONSTANT DATA        */
    #else 
        .const      : {} >> FLASH2 | FLASH    /* CONSTANT DATA        */ 
    #endif 

    .cio        : {} > RAM                /* C I/O BUFFER                      */
	
	.infoA     : {} > INFOA              /* MSP430 INFO FLASH Memory segments */
    .infoB     : {} > INFOB
    .infoC     : {} > INFOC
    .infoD     : {} > INFOD

    .APP_PROXY_VECTORS : {} > APP_PROXY_VECTORS /* INTERRUPT PROXY TABLE            */
    .reset       : {}               > RESET  /* MSP430 RESET VECTOR                 */
}

/****************************************************************************/
/* INCLUDE PERIPHERALS MEMORY MAP                                           */
/****************************************************************************/

-l MSP430F6779A.cmd

the following is my 24Bit sigma delta interrupt

 

#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=SD24B_VECTOR
__interrupt void SD24BISR(void) {
#elif defined(__GNUC__)
void __attribute__ ((interrupt(SD24_VECTOR))) SD24_ISR(void)
#else
#error Compiler not supported!
#endif
    int16_t tempV;
    int32_t tempI;
    switch(SD24BIV)
    {
    case SD24BIV_SD24IFG0:                  // SD24MEM0 IFG
        chReadStatus |= HAL_ADC_CH0_READ;

        // Store Voltage Results
        phAVSamples[phAWriteVIdx] = SD24_B_getHighWordResults(SD24_BASE, SD24_B_CONVERTER_0);

        // Apply Voltage DC Filter
        tempV = EM_voltageDCFilter(&gEmSWResult.phaseBGResults[EM_PH_A_IDX].vDCEstimate, phAVSamples[phAWriteVIdx]);
        phAVSamples[phAWriteVIdx] = tempV;

        // Increase Index and Mask
        phAWriteVIdx = (phAWriteVIdx+1) & (HAL_ADC_V_MASK);
        break;
    case SD24BIV_SD24IFG1:                  // SD24MEM1 IFG
        chReadStatus |= HAL_ADC_CH1_READ;

        // Store Voltage Results
        phBVSamples[phBWriteVIdx] = SD24_B_getHighWordResults(SD24_BASE, SD24_B_CONVERTER_1);

        // Apply Voltage DC Filter
        tempV = EM_voltageDCFilter(&gEmSWResult.phaseBGResults[EM_PH_B_IDX].vDCEstimate, phBVSamples[phBWriteVIdx]);
        phBVSamples[phBWriteVIdx] = tempV;

        // Increase Index and Mask
        phBWriteVIdx = (phBWriteVIdx+1) & (HAL_ADC_V_MASK);
        break;
    case SD24BIV_SD24IFG2:                  // SD24MEM2 IFG
        chReadStatus |= HAL_ADC_CH2_READ;

        // Store Voltage Results
        phCVSamples[phCWriteVIdx] = SD24_B_getHighWordResults(SD24_BASE, SD24_B_CONVERTER_2);

        // Apply Voltage DC Filter
        tempV = EM_voltageDCFilter(&gEmSWResult.phaseBGResults[EM_PH_C_IDX].vDCEstimate, phCVSamples[phCWriteVIdx]);
        phCVSamples[phCWriteVIdx] = tempV;

        // Increase Index and Mask
        phCWriteVIdx = (phCWriteVIdx+1) & (HAL_ADC_V_MASK);
        break;
    case SD24BIV_SD24IFG3:                  // SD24MEM3 IFG
        break;
    case SD24BIV_SD24IFG4:                  // SD24MEM4 IFG
        chReadStatus |= HAL_ADC_CH4_READ;

        // Store Current Results
        phAISamples[phAWriteIIdx] = SD24_B_getResults(SD24_BASE, SD24_B_CONVERTER_4);
        tempI = phAISamples[phAWriteIIdx] >> 1;
        phAISamples[phAWriteIIdx] = tempI;

        // Apply Current DC Filter
        tempI = EM_currentDCFilter(gEmSWResult.phaseBGResults[EM_PH_A_IDX].iDCEstimate, phAISamples[phAWriteIIdx]);
        phAISamples[phAWriteIIdx] = tempI;

        // Increase Index and Mask
        phAWriteIIdx = (phAWriteIIdx+1) & (HAL_ADC_I_MASK);
        break;
    case SD24BIV_SD24IFG5:                  // SD24MEM5 IFG
        chReadStatus |= HAL_ADC_CH5_READ;

        // Store Current Results
        phBISamples[phBWriteIIdx] = SD24_B_getResults(SD24_BASE, SD24_B_CONVERTER_5);
        tempI = phBISamples[phBWriteIIdx] >> 1;
        phBISamples[phBWriteIIdx] = tempI;

        // Apply Current DC Filter
        tempI = EM_currentDCFilter(gEmSWResult.phaseBGResults[EM_PH_B_IDX].iDCEstimate, phBISamples[phBWriteIIdx]);
        phBISamples[phBWriteIIdx] = tempI;

        // Increase Index and Mask
        phBWriteIIdx = (phBWriteIIdx+1) & (HAL_ADC_I_MASK);
        break;
    case SD24BIV_SD24IFG6:                  // SD24MEM6 IFG
        chReadStatus |= HAL_ADC_CH6_READ;

        // Store Current Results
        phCISamples[phCWriteIIdx] = SD24_B_getResults(SD24_BASE, SD24_B_CONVERTER_6);
        tempI = phCISamples[phCWriteIIdx] >> 1;
        phCISamples[phCWriteIIdx] = tempI;

        // Apply Current DC Filter
        tempI = EM_currentDCFilter(gEmSWResult.phaseBGResults[EM_PH_C_IDX].iDCEstimate, phCISamples[phCWriteIIdx]);
        phCISamples[phCWriteIIdx] = tempI;

        // Increase Index and Mask
        phCWriteIIdx = (phCWriteIIdx+1) & (HAL_ADC_I_MASK);
        break;
    default: break;
    }

    // Check if both channels were read for all phases
    if((chReadStatus & (HAL_ADC_CH0_READ+HAL_ADC_CH1_READ+HAL_ADC_CH2_READ+HAL_ADC_CH4_READ+HAL_ADC_CH5_READ+HAL_ADC_CH6_READ)) == 
       (HAL_ADC_CH0_READ+HAL_ADC_CH1_READ+HAL_ADC_CH2_READ+HAL_ADC_CH4_READ+HAL_ADC_CH5_READ+HAL_ADC_CH6_READ))
    {
        chReadStatus = 0;

        // Pulse Generation for Total Energy
        if(phASA == 0 || phBSA == 0 || phCSA == 0)
        {
            // Check Energy and Generate Pulses
            EM_genPulseTotalPhases(gEmSWConfig.systemConfig,
                                     &gEmSWConfig.systemConfig->pulseArray[EM_PH_TOTAL_IDX],
                                     gEmSWResult.emTotalResult);
        }
        // Phase A Data Processing
        if(phASA == 0)
        {
            // Voltage aligned with Current
            if(phAProc == 0)
            {
                phAProc = 1;
            }
            else
            {
                // Increase Current (I) Index and Mask
                phAIIdx = (phAIIdx+1) & HAL_ADC_I_MASK;

                // Increase Voltage (V) Index and Mask
                phAVIdx = (phAVIdx+1) & HAL_ADC_V_MASK;
            }

            // Set the Ptrs to voltage and current
            emPhaseConfiguration[EM_PH_A_IDX].voltageSamplePtr = &phAVSamples[phAVIdx];
            emPhaseConfiguration[EM_PH_A_IDX].currentSamplePtr = &phAISamples[phAIIdx];

            // Process the samples
            EM_perSampleProc(gEmSWResult.phaseMetrologyPing[EM_PH_A_IDX],
                             &gEmSWConfig.meterConfig->phaseConfigPtr[EM_PH_A_IDX],
                             &gEmSWResult.phaseBGResults[EM_PH_A_IDX]);

            // Check Energy and Generate Pulses
            EM_genPulseIndPhase(gEmSWConfig.systemConfig,
                                &gEmSWConfig.systemConfig->pulseArray[EM_PH_A_IDX],
                                &gEmSWResult.phaseResults[EM_PH_A_IDX]);

            if(gEmSWResult.phaseMetrologyPing[EM_PH_A_IDX]->cycleCount == gEmSWConfig.algorithmConfig->mainNomFreq)
            {
                phaseDataReady |= HAL_ADC_PHASE_A_DATA_READY;
                EM_perDataChunk(&gEmSWConfig, (EM_SW_Lib_Result_Handle *) &gEmSWResult, EM_PH_A_IDX);
            }
            else if (gEmSWResult.phaseMetrologyPing[EM_PH_A_IDX]->sampleCount > (2*EM_SAMPLING_FREQ_HZ))
            {
                phaseDataReady |= HAL_ADC_PHASE_A_DATA_READY;
                EM_perDataChunk(&gEmSWConfig, (EM_SW_Lib_Result_Handle *) &gEmSWResult, EM_PH_A_IDX);
            }
        }
        else if(phASA > 0)
        {
            // Voltage leading Current
            phASA = phASA-1;
            phAIIdx = phAIIdx+1;
        }
        else
        {
            // Voltage lagging Current
            phASA = phASA+1;
            phAVIdx = phAVIdx+1;
        }
        // Phase B Data Processing
        if(phBSA == 0)
        {
            // Voltage aligned with Current
            if(phBProc == 0)
            {
                phBProc = 1;
            }
            else
            {
                // Increase Current (I) Index and Mask
                phBIIdx = (phBIIdx+1) & HAL_ADC_I_MASK;

                // Increase Voltage (V) Index and Mask
                phBVIdx = (phBVIdx+1) & HAL_ADC_V_MASK;
            }

            // Set the Ptrs to voltage and current
            emPhaseConfiguration[EM_PH_B_IDX].voltageSamplePtr = &phBVSamples[phBVIdx];
            emPhaseConfiguration[EM_PH_B_IDX].currentSamplePtr = &phBISamples[phBIIdx];

            // Process the samples
            EM_perSampleProc(gEmSWResult.phaseMetrologyPing[EM_PH_B_IDX],
                             &gEmSWConfig.meterConfig->phaseConfigPtr[EM_PH_B_IDX],
                             &gEmSWResult.phaseBGResults[EM_PH_B_IDX]);

            // Check Energy and Generate Pulses
            EM_genPulseIndPhase(gEmSWConfig.systemConfig,
                                &gEmSWConfig.systemConfig->pulseArray[EM_PH_B_IDX],
                                &gEmSWResult.phaseResults[EM_PH_B_IDX]);

            if(gEmSWResult.phaseMetrologyPing[EM_PH_B_IDX]->cycleCount == gEmSWConfig.algorithmConfig->mainNomFreq)
            {
                phaseDataReady |= HAL_ADC_PHASE_B_DATA_READY;
                EM_perDataChunk(&gEmSWConfig, (EM_SW_Lib_Result_Handle *) &gEmSWResult, EM_PH_B_IDX);
            }
            else if (gEmSWResult.phaseMetrologyPing[EM_PH_B_IDX]->sampleCount > (2*EM_SAMPLING_FREQ_HZ))
            {
                phaseDataReady |= HAL_ADC_PHASE_B_DATA_READY;
                EM_perDataChunk(&gEmSWConfig, (EM_SW_Lib_Result_Handle *) &gEmSWResult, EM_PH_B_IDX);
            }
        }
        else if(phBSA > 0)
        {
            // Voltage leading Current
            phBSA = phBSA-1;
            phBIIdx = phBIIdx+1;
        }
        else
        {
            // Voltage lagging Current
            phBSA = phBSA+1;
            phBVIdx = phBVIdx+1;
        }
        // Phase C Data Processing
        if(phCSA == 0)
        {
            // Voltage aligned with Current
            if(phCProc == 0)
            {
                phCProc = 1;
            }
            else
            {
                // Increase Current (I) Index and Mask
                phCIIdx = (phCIIdx+1) & HAL_ADC_I_MASK;

                // Increase Voltage (V) Index and Mask
                phCVIdx = (phCVIdx+1) & HAL_ADC_V_MASK;
            }

            // Set the Ptrs to voltage and current
            emPhaseConfiguration[EM_PH_C_IDX].voltageSamplePtr = &phCVSamples[phCVIdx];
            emPhaseConfiguration[EM_PH_C_IDX].currentSamplePtr = &phCISamples[phCIIdx];

            // Process the samples
            EM_perSampleProc(gEmSWResult.phaseMetrologyPing[EM_PH_C_IDX],
                             &gEmSWConfig.meterConfig->phaseConfigPtr[EM_PH_C_IDX],
                             &gEmSWResult.phaseBGResults[EM_PH_C_IDX]);

            // Check Energy and Generate Pulses
            EM_genPulseIndPhase(gEmSWConfig.systemConfig,
                                &gEmSWConfig.systemConfig->pulseArray[EM_PH_C_IDX],
                                &gEmSWResult.phaseResults[EM_PH_C_IDX]);

            if(gEmSWResult.phaseMetrologyPing[EM_PH_C_IDX]->cycleCount == gEmSWConfig.algorithmConfig->mainNomFreq)
            {
                phaseDataReady |= HAL_ADC_PHASE_C_DATA_READY;
                EM_perDataChunk(&gEmSWConfig, (EM_SW_Lib_Result_Handle *) &gEmSWResult, EM_PH_C_IDX);
            }
            else if (gEmSWResult.phaseMetrologyPing[EM_PH_C_IDX]->sampleCount > (2*EM_SAMPLING_FREQ_HZ))
            {
                phaseDataReady |= HAL_ADC_PHASE_C_DATA_READY;
                EM_perDataChunk(&gEmSWConfig, (EM_SW_Lib_Result_Handle *) &gEmSWResult, EM_PH_C_IDX);
            }
        }
        else if(phCSA > 0)
        {
            // Voltage leading Current
            phCSA = phCSA-1;
            phCIIdx = phCIIdx+1;
        }
        else
        {
            // Voltage lagging Current
            phCSA = phCSA+1;
            phCVIdx = phCVIdx+1;
        }
    }
}

the following is how my vector table is defined in file TI_MSPBoot_Mgr_Vectors_F6779A.c which was generated using MSPBoot

/******************************************************************************/
/* Vector Redirection FILE FOR MSPBoot Application USING MSP430F6779A  */
/* File generated with MSPBootVecRedGen.pl on 07-01-2024 */
/*----------------------------------------------------------------------------*/

#include "msp430.h"
#include <stdint.h>
#include "TI_MSPBoot_Mgr_Vectors.h"

// Global variables
/*! Password sent by Application to force boot mode. This variable is in a fixed
    location and should keep same functionality and location in Boot and App */
extern uint16_t  PassWd;

/*! Status and Control byte. This variable is in a fixed
    location and should keep same functionality and location in Boot and App */
extern uint8_t  StatCtrl;

/******************************************************************************
 *
 * @brief   Forces Boot mode
 *  Sets a bit in Status and Control byte to request Boot mode, writes a password
 *  in PassWd and forces a PUC reset
 *  Boot will start execution after PUC and detect forced Boot mode
 *
 * @return  none
 *****************************************************************************/
void TI_MSPBoot_JumpToBoot( void )
{
    PassWd = BSL_PASSWORD;      // Send password
    StatCtrl |= BOOT_APP_REQ;   // Set flag to request boot mode
    __disable_interrupt();      // Disable all interrupts
    WDTCTL = WDT_MRST_0_064;    // Set watchdog and wait for expiration
    while (1);
}

//
//  External ISR prototypes used by ProxyVectorTable
//  Add your own ISRs as shown below
//
//TODO: Add extern prototypes of every ISR in your system
extern __interrupt void Dummy_Isr (void);
extern __interrupt void RTC_ISR (void);
extern __interrupt void PORT1_ISR (void);
extern __interrupt void PORT2_ISR (void);
extern __interrupt void DMA_ISR (void);
extern __interrupt void TIMER0_A0_ISR (void);
extern __interrupt void USCI_A2_ISR (void);
extern __interrupt void USCI_B1_ISR (void);
extern __interrupt void UART_ISR (void);
extern __interrupt void WDT_ISR (void);
extern __interrupt void UNMI_ISR (void);
extern __interrupt void SD24BISR (void);
#ifdef SHARED_PI
extern __interrupt void TI_MSPBoot_Comm_Isr(void);
#endif


//
//  Constant tables
//
/*! This is a "proxy" interrupt table which is used by the bootloader to jump to
    each interrupt routine.
    It always resides in the same location.
    It contains a BRA instruction (0x4030) followed by the address of each
    vector routine.
    Unimplemented vectors are removed (and unused vectors can be removed too)
    to save flash space
*/
////TODO: Update with the interrupt vectors used in your application, see examples
//#pragma DATA_SECTION(ProxyVectorTable, ".APP_PROXY_VECTORS")
//#pragma RETAIN(ProxyVectorTable)
//const uint16_t ProxyVectorTable[] =
//{
//    0x4030, (uint16_t) DUMMY_ISR,           // APP_PROXY_VECTOR(0)  AES
//    0x4030, (uint16_t) DUMMY_ISR,           // APP_PROXY_VECTOR(1)  COMP_B
//    0x4030, (uint16_t) RTC_ISR,                 // APP_PROXY_VECTOR(2)  RTC
//    0x4030, (uint16_t) DUMMY_ISR,           // APP_PROXY_VECTOR(3)  LCD_C
//    0x4030, (uint16_t) DUMMY_ISR,           // APP_PROXY_VECTOR(4)  TIMER3_A1
//    0x4030, (uint16_t) DUMMY_ISR,           // APP_PROXY_VECTOR(5)  TIMER3_A0
//    0x4030, (uint16_t) PORT2_ISR,           // APP_PROXY_VECTOR(6)  PORT2
//    0x4030, (uint16_t) DUMMY_ISR,           // APP_PROXY_VECTOR(7)  TIMER2_A1
//    0x4030, (uint16_t) DUMMY_ISR,           // APP_PROXY_VECTOR(8)  TIMER2_A0
//    0x4030, (uint16_t) PORT1_ISR,           // APP_PROXY_VECTOR(9)  PORT1
//    0x4030, (uint16_t) USCI_B1_ISR,           // APP_PROXY_VECTOR(10)  USCI_B1
//    0x4030, (uint16_t) DUMMY_ISR,           // APP_PROXY_VECTOR(11)  USCI_A3
//    0x4030, (uint16_t) DUMMY_ISR,           // APP_PROXY_VECTOR(12)  TIMER1_A1
//    0x4030, (uint16_t) DUMMY_ISR,           // APP_PROXY_VECTOR(13)  TIMER1_A0
//    0x4030, (uint16_t) DMA_ISR,           // APP_PROXY_VECTOR(14)  DMA
//    0x4030, (uint16_t) DUMMY_ISR,           // APP_PROXY_VECTOR(15)  AUX
//    0x4030, (uint16_t) USCI_A2_ISR,           // APP_PROXY_VECTOR(16)  USCI_A2
//    0x4030, (uint16_t) DUMMY_ISR,           // APP_PROXY_VECTOR(17)  USCI_A1
//    0x4030, (uint16_t) DUMMY_ISR,           // APP_PROXY_VECTOR(18)  TIMER0_A1
//    0x4030, (uint16_t) TIMER0_A0_ISR,           // APP_PROXY_VECTOR(19)  TIMER0_A0
//    0x4030, (uint16_t) SD24BISR,           // APP_PROXY_VECTOR(20)  SD24B
//    0x4030, (uint16_t) DUMMY_ISR,           // APP_PROXY_VECTOR(21)  ADC10
//    0x4030, (uint16_t) DUMMY_ISR,           // APP_PROXY_VECTOR(22)  USCI_B0
//    0x4030, (uint16_t) UART_ISR,           // APP_PROXY_VECTOR(23)  USCI_A0
//    0x4030, (uint16_t) WDT_ISR,           // APP_PROXY_VECTOR(24)  WDT
//    0x4030, (uint16_t) UNMI_ISR,           // APP_PROXY_VECTOR(25)  UNMI
//    0x4030, (uint16_t) DUMMY_ISR,           // APP_PROXY_VECTOR(26)  SYSNMI
//};

//TODO: Update with the interrupt vectors used in your application, see examples
#pragma DATA_SECTION(ProxyVectorTable, ".APP_PROXY_VECTORS")
#pragma RETAIN(ProxyVectorTable)
const uint16_t ProxyVectorTable[] =
{
    0x4030, (uint16_t) Dummy_Isr,           // APP_PROXY_VECTOR(0)  AES
    0x4030, (uint16_t) Dummy_Isr,           // APP_PROXY_VECTOR(1)  COMP_B
    0x4030, (uint16_t) RTC_ISR,           // APP_PROXY_VECTOR(2)  RTC
    0x4030, (uint16_t) Dummy_Isr,           // APP_PROXY_VECTOR(3)  LCD_C
    0x4030, (uint16_t) Dummy_Isr,           // APP_PROXY_VECTOR(4)  TIMER3_A1
    0x4030, (uint16_t) Dummy_Isr,           // APP_PROXY_VECTOR(5)  TIMER3_A0
    0x4030, (uint16_t) PORT2_ISR,           // APP_PROXY_VECTOR(6)  PORT2
    0x4030, (uint16_t) Dummy_Isr,           // APP_PROXY_VECTOR(7)  TIMER2_A1
    0x4030, (uint16_t) Dummy_Isr,           // APP_PROXY_VECTOR(8)  TIMER2_A0
    0x4030, (uint16_t) PORT1_ISR,           // APP_PROXY_VECTOR(9)  PORT1
    0x4030, (uint16_t) USCI_B1_ISR,           // APP_PROXY_VECTOR(10)  USCI_B1
    0x4030, (uint16_t) Dummy_Isr,           // APP_PROXY_VECTOR(11)  USCI_A3
    0x4030, (uint16_t) Dummy_Isr,           // APP_PROXY_VECTOR(12)  TIMER1_A1
    0x4030, (uint16_t) Dummy_Isr,           // APP_PROXY_VECTOR(13)  TIMER1_A0
    0x4030, (uint16_t) DMA_ISR,           // APP_PROXY_VECTOR(14)  DMA
    0x4030, (uint16_t) Dummy_Isr,           // APP_PROXY_VECTOR(15)  AUX
    0x4030, (uint16_t) USCI_A2_ISR,           // APP_PROXY_VECTOR(16)  USCI_A2
    0x4030, (uint16_t) Dummy_Isr,           // APP_PROXY_VECTOR(17)  USCI_A1
    0x4030, (uint16_t) Dummy_Isr,           // APP_PROXY_VECTOR(18)  TIMER0_A1
    0x4030, (uint16_t) TIMER0_A0_ISR,           // APP_PROXY_VECTOR(19)  TIMER0_A0
    0x4030, (uint16_t) SD24BISR,           // APP_PROXY_VECTOR(20)  SD24B
    0x4030, (uint16_t) Dummy_Isr,           // APP_PROXY_VECTOR(21)  ADC10
    0x4030, (uint16_t) Dummy_Isr,           // APP_PROXY_VECTOR(22)  USCI_B0
    0x4030, (uint16_t) UART_ISR,           // APP_PROXY_VECTOR(23)  USCI_A0
    0x4030, (uint16_t) WDT_ISR,           // APP_PROXY_VECTOR(24)  WDT
    0x4030, (uint16_t) UNMI_ISR,           // APP_PROXY_VECTOR(25)  UNMI
    0x4030, (uint16_t) Dummy_Isr,           // APP_PROXY_VECTOR(26)  SYSNMI
};

I am also getting the below given warning in this file 

  • orignally in linker script .cinit      : {} > FLASH but i changed it to .cinit      : {} > FLASH | FLASH2 as my code was not fitting into the flash segment as my total code size is 50kb and the partition made by msp boot is of only 9kb in flash 

    and I have also tried enabling large code model and i am using code composer studio

  • this is my memory view

  • Hi Jitain,

    I suggest you should firstly debug where the code hange out, this could help you quickly eliminate some reasons. Please share your feedback and I can further give some feedback.

    orignally in linker script .cinit      : {} > FLASH but i changed it to .cinit      : {} > FLASH | FLASH2 as my code was not fitting into the flash segment as my total code size is 50kb and the partition made by msp boot is of only 9kb in flash 

    and I have also tried enabling large code model and i am using code composer studio

    Yes, it could.

    Could you share what's your application linker file? I don't know whether you application linker and boot linker has some conflicts. Then cause some issues.

    As for MSPBOOT, I doesn't use it before. So, let us focus on other aspects firstly.

    B.R.

    Sal

  • Hi Sal I was able to resolve the issue my text section was getting divided in 2 parts text 1 which wash Part of Flash and text 2 which was part of flash 2 so now i made changes in linker file to keep cinit const and text:_isr in flash and the whole text section in Flash 2 that solved my issue 

    (I had to do it because bootloader made my flash section to 9 kb while text section was 50kb, so i tried to split the section into flash | flash2 as you can see in the linkerscript attached in my question)

    thoug i have attached my linker file earlier 

  • Hi Jitain,

    I had always thought this was a bootloader project, it seems I misunderstood the project, it is the application one.

    It is good to know you have solved the issue, thanks for your update. I will close the thread.

    B.R.

    Sal

  • Hi Sal, 

    it was a bootloader compatible application that i was having the issue with. the application was working fine when used independently but when it was coverted into bootloader compatible application there was this issue 
    but Anyways thanks for your time and response I really appreciate your support 

**Attention** This is a public forum