Tool/software:
Hi
I think SPI data pin status after communication (not driving by eUSCI peripheral) is defined PxREN & PxOUT register.
Is the clock pin (UCA1CLK) same (in master mode)?
Thanks,
GR
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi
I think SPI data pin status after communication (not driving by eUSCI peripheral) is defined PxREN & PxOUT register.
Is the clock pin (UCA1CLK) same (in master mode)?
Thanks,
GR
When the pin is connected to the SPI unit, the SPI "standard" (such as it is) says that SCK is driven (all the time). If the SPI is idle, it is driven according to the clock polarity.
If the pin is disconnected from the SPI (PSEL = 00), it's not an SPI pin any more, so it's controlled by the PxDIR/PxREN/PxOUT settings.
[Edit: Minor correction.]
Hi Janz, Bruce,
Thanks for your supporting.
I want to confirm with whether you want to know the voltage level of SPI clock pin or you want to know how to modification the configurate of the SPI clock pin after communication.
I want to know SPI clock pin output voltage when not active communication.
If the SPI is idle, it is driven according to the clock polarity.
Thanks for information.I underatand.
SPI clock line level is define by clock polarity setting.
Best regards,
GR
**Attention** This is a public forum