Other Parts Discussed in Thread: MSP-FET
Tool/software:
hi,
we are using the BSL-ROCKET with the EVM430-FR6047 and the BSL-scripter software
this is my hookup:

and here is the EVM

i am using the JTAG connector to scope the TX, RX,RST, and TEST signals.
kindly confirm setup.
i am giving calling the following script to perform a mass erase:
LOG
MODE FRxx UART 9600 COM10
DELAY 100
VERBOSE
MASS_ERASE
i receive the following:
---------------------------------------------------------
BSL Scripter 3.4.0.1
PC software for BSL programming
2024-Jul-31 13:05:50
---------------------------------------------------------
Input file script is : C:/Users/ephra/Dropbox/Desktop/MSP430-BSL/progevm-UART-me.txt
LOG
MODE FRxx UART 9600 COM10
DELAY 100
Delay 100 ms
VERBOSE
Verbose mode is now on!
MASS_ERASE
[80] [01] [00] [15] [64] [a3]
[ACK_ERROR_MESSAGE]Unknown ACK value!
kindly elaborate on the issues with the TI tools.
Br.
Ephraim
thanks,