This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2433: Custom BSL using linker file for interrupt vector mapping

Part Number: MSP430FR2433

Tool/software:

Hello,

Here need to do custom BSL

1. First time flashing with the uniflasher load binary file of boot loader at some address and application binary at another address. 

         --> In the linker file having the copy of vector information at the information memory address.

2. From the second the onwards boot loader should the following 

          --> whenever there is any update either text or vector info,

           --> then if there is any update in the vector information, update the same with the information memory 

          --> Then execute the application binary 

The issue facing for the above scenario unable to update the RESET information to two different locations. Any one location alone getting updated with reset information.

Thanks in advance.

  • Hi,

    I am not totally understand what you mean by the RESET information? Could you explain more about it? 

    Why you need reset for two different locations? And by locations, does it mean the memory of boot code, app code and information code memory?

    Best regards,

    Cash Hao

  • Hi,

    I have customized boot code and app code. both are pointing the same address of .reset vector.  

    Here is the scenario,

    In my flash memory

    1. 0XC400 address contains boot code with some bytes 

    2. 0xD800 address contains app code with some bytes.

    if there is a firmware update request it's always pointing to the app reset vector address.

    for boot code also same reset vector address.

    my requirement is like it has to run the boot loader and then update the app code, but it's not happening so decided to have the back of both code vector information into the information memory and then access the respective code based the request raised.

    Thanks.  

  • Hi,

    Since your boot code start at 0xC400 which is the start address of FRAM. By default, when you power up the MCU, it will first runs into your boot code. 

    In boot code you can determine to run app code or not. If you need to run app code, you can directly set the PC to 0xD800 which is the start address of app code. Then the MCU will run into app code. 

    If you want to jump to boot code in app code, you can directly SW reset the MCU. Then it will start with boot code again. I do not think  set two reset vector address is needed in this case.

    Best regards,

    Cash Hao

  • Hi,

    My request is, I want to write bootloader code and application code for the specified address with fresh microcontroller during manufacturing time via uniflasher tool. Then the microcontroller is in field the firmware update should be via bootloader. 

    For the MSP430FR2433 microcontroller, we have application code and customized bootloader code.

    1. 0XC400 address contains boot code with some bytes 

    2. 0xD800 address contains app code with some bytes.

    3. For both code the reset vector address is 0x FFFE.

    The problem is, when we had flashed the binary via UNIFLASHER tool for the above specified address for the first time. 

    Then, to update the binary using bootloader, reset vector address 0x FFFE is pointing to the main application, and it is not pointing to the bootloader code.

    So, decide to locate the reset vector information with the INFO memory using the linker command. please find the below linker command for your reference. 

    /* ============================================================================ */
    /* Copyright (c) 2020, Texas Instruments Incorporated */
    /* All rights reserved. */
    /* */
    /* Redistribution and use in source and binary forms, with or without */
    /* modification, are permitted provided that the following conditions */
    /* are met: */
    /* */
    /* * Redistributions of source code must retain the above copyright */
    /* notice, this list of conditions and the following disclaimer. */
    /* */
    /* * Redistributions in binary form must reproduce the above copyright */
    /* notice, this list of conditions and the following disclaimer in the */
    /* documentation and/or other materials provided with the distribution. */
    /* */
    /* * Neither the name of Texas Instruments Incorporated nor the names of */
    /* its contributors may be used to endorse or promote products derived */
    /* from this software without specific prior written permission. */
    /* */
    /* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" */
    /* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, */
    /* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR */
    /* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR */
    /* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, */
    /* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, */
    /* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; */
    /* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, */
    /* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR */
    /* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, */
    /* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */
    /* ============================================================================ */

    /******************************************************************************/
    /* lnk_msp430fr2433.cmd - LINKER COMMAND FILE FOR LINKING MSP430FR2433 PROGRAMS */
    /* */
    /* Usage: lnk430 <obj files...> -o <out file> -m <map file> lnk.cmd */
    /* cl430 <src files...> -z -o <out file> -m <map file> lnk.cmd */
    /* */
    /*----------------------------------------------------------------------------*/
    /* These linker options are for command line linking only. For IDE linking, */
    /* you should set your linker options in Project Properties */
    /* -c LINK USING C CONVENTIONS */
    /* -stack 0x0100 SOFTWARE STACK SIZE */
    /* -heap 0x0100 HEAP AREA SIZE */
    /* */
    /*----------------------------------------------------------------------------*/
    /* Version: 1.213 */
    /*----------------------------------------------------------------------------*/

    /****************************************************************************/
    /* Specify the system memory map */
    /****************************************************************************/

    MEMORY
    {
    SFR : origin = 0x0000, length = 0x0010
    PERIPHERALS_8BIT : origin = 0x0010, length = 0x00F0
    PERIPHERALS_16BIT : origin = 0x0100, length = 0x0100
    RAM : origin = 0x2000, length = 0x1000
    INFOA : origin = 0x1800, length = 0x0200
    FRAM : origin = 0xD800, length = 0x1400 //0x3B80
    JTAGSIGNATURE : origin = 0xFF80, length = 0x0004, fill = 0xFFFF
    BSLSIGNATURE : origin = 0xFF84, length = 0x0004, fill = 0xFFFF
    INT00 : origin = 0xFF88, length = 0x0002
    INT01 : origin = 0xFF8A, length = 0x0002
    INT02 : origin = 0xFF8C, length = 0x0002
    INT03 : origin = 0xFF8E, length = 0x0002
    INT04 : origin = 0xFF90, length = 0x0002
    INT05 : origin = 0xFF92, length = 0x0002
    INT06 : origin = 0xFF94, length = 0x0002
    INT07 : origin = 0xFF96, length = 0x0002
    INT08 : origin = 0xFF98, length = 0x0002
    INT09 : origin = 0xFF9A, length = 0x0002
    INT10 : origin = 0xFF9C, length = 0x0002
    INT11 : origin = 0xFF9E, length = 0x0002
    INT12 : origin = 0xFFA0, length = 0x0002
    INT13 : origin = 0xFFA2, length = 0x0002
    INT14 : origin = 0xFFA4, length = 0x0002
    INT15 : origin = 0xFFA6, length = 0x0002
    INT16 : origin = 0xFFA8, length = 0x0002
    INT17 : origin = 0xFFAA, length = 0x0002
    INT18 : origin = 0xFFAC, length = 0x0002
    INT19 : origin = 0xFFAE, length = 0x0002
    INT20 : origin = 0xFFB0, length = 0x0002
    INT21 : origin = 0xFFB2, length = 0x0002
    INT22 : origin = 0xFFB4, length = 0x0002
    INT23 : origin = 0xFFB6, length = 0x0002
    INT24 : origin = 0xFFB8, length = 0x0002
    INT25 : origin = 0xFFBA, length = 0x0002
    INT26 : origin = 0xFFBC, length = 0x0002
    INT27 : origin = 0xFFBE, length = 0x0002
    INT28 : origin = 0xFFC0, length = 0x0002
    INT29 : origin = 0xFFC2, length = 0x0002
    INT30 : origin = 0xFFC4, length = 0x0002
    INT31 : origin = 0xFFC6, length = 0x0002
    INT32 : origin = 0xFFC8, length = 0x0002
    INT33 : origin = 0xFFCA, length = 0x0002
    INT34 : origin = 0xFFCC, length = 0x0002
    INT35 : origin = 0xFFCE, length = 0x0002
    INT36 : origin = 0xFFD0, length = 0x0002
    INT37 : origin = 0xFFD2, length = 0x0002
    INT38 : origin = 0xFFD4, length = 0x0002
    INT39 : origin = 0xFFD6, length = 0x0002
    INT40 : origin = 0xFFD8, length = 0x0002
    INT41 : origin = 0xFFDA, length = 0x0002
    INT42 : origin = 0xFFDC, length = 0x0002
    INT43 : origin = 0xFFDE, length = 0x0002
    INT44 : origin = 0xFFE0, length = 0x0002
    INT45 : origin = 0xFFE2, length = 0x0002
    INT46 : origin = 0xFFE4, length = 0x0002
    INT47 : origin = 0xFFE6, length = 0x0002
    INT48 : origin = 0xFFE8, length = 0x0002
    INT49 : origin = 0xFFEA, length = 0x0002
    INT50 : origin = 0xFFEC, length = 0x0002
    INT51 : origin = 0xFFEE, length = 0x0002
    INT52 : origin = 0xFFF0, length = 0x0002
    INT53 : origin = 0xFFF2, length = 0x0002
    INT54 : origin = 0xFFF4, length = 0x0002
    INT55 : origin = 0xFFF6, length = 0x0002
    INT56 : origin = 0xFFF8, length = 0x0002
    INT57 : origin = 0xFFFA, length = 0x0002
    INT58 : origin = 0xFFFC, length = 0x0002
    RESET : origin = 0xFFFE, length = 0x0002
    }

    /****************************************************************************/
    /* Specify the sections allocation into memory */
    /****************************************************************************/

    SECTIONS
    {
    GROUP(ALL_FRAM)
    {
    GROUP(READ_WRITE_MEMORY)
    {
    .TI.persistent : {} /* For #pragma persistent */
    }

    GROUP(READ_ONLY_MEMORY)
    {
    .cinit : {} /* Initialization tables */
    .pinit : {} /* C++ constructor tables */
    .binit : {} /* Boot-time Initialization tables */
    .init_array : {} /* C++ constructor tables */
    .mspabi.exidx : {} /* C++ constructor tables */
    .mspabi.extab : {} /* C++ constructor tables */
    .const : {} /* Constant data */
    }

    GROUP(EXECUTABLE_MEMORY)
    {
    .text : {} /* Code */
    }
    } > FRAM

    #ifdef __TI_COMPILER_VERSION__
    #if __TI_COMPILER_VERSION__ >= 15009000
    #ifndef __LARGE_CODE_MODEL__
    .TI.ramfunc : {} load=FRAM, run=RAM, table(BINIT)
    #else
    .TI.ramfunc : {} load=FRAM | FRAM2, run=RAM, table(BINIT)
    #endif
    #endif
    #endif

    .jtagsignature : {} > JTAGSIGNATURE /* JTAG Signature */
    .bslsignature : {} > BSLSIGNATURE /* BSL Signature */

    .bss : {} > RAM /* Global & static vars */
    .data : {} > RAM /* Global & static vars */
    .TI.noinit : {} > RAM /* For #pragma noinit */
    .cio : {} > RAM /* C I/O buffer */
    .sysmem : {} > RAM /* Dynamic memory allocation area */
    .stack : {} > RAM (HIGH) /* Software system stack */

    //.jtagsignature : {} > 0x1830 /* MSP430 Jtag signature copyed to info memory */
    /*.bslsignature : {} > 0x1834
    PORT2 : {} > 0x1838
    PORT1 : {} > 0x183A
    ADC : {} > 0x183C
    USCI_B0 : {} > 0x183E
    USCI_A1 : {} > 0x1840
    USCI_A0 : {} > 0x1842
    WDT : {} > 0x1844
    RTC : {} > 0x1846
    TIMER3_A1 : {} > 0x1848
    TIMER3_A0 : {} > 0x184A
    TIMER2_A1 : {} > 0x184C
    TIMER2_A0 : {} > 0x184E
    TIMER1_A1 : {} > 0x1850
    TIMER1_A0 : {} > 0x1852
    TIMER0_A1 : {} > 0x1854
    TIMER0_A0 : {} > 0x1856
    UNMI : {} > 0x1858
    SYSNMI : {} > 0x185A
    .reset : {} > 0x185C */ /* MSP43O reset vector copyed to info memory */

    // .infoA (NOLOAD) : {} > INFOA /* MSP430 INFO FRAM Memory segments */

    /* MSP430 Interrupt vectors */
    .int00 : {} > INT00
    .int01 : {} > INT01
    .int02 : {} > INT02
    .int03 : {} > INT03
    .int04 : {} > INT04
    .int05 : {} > INT05
    .int06 : {} > INT06
    .int07 : {} > INT07
    .int08 : {} > INT08
    .int09 : {} > INT09
    .int10 : {} > INT10
    .int11 : {} > INT11
    .int12 : {} > INT12
    .int13 : {} > INT13
    .int14 : {} > INT14
    .int15 : {} > INT15
    .int16 : {} > INT16
    .int17 : {} > INT17
    .int18 : {} > INT18
    .int19 : {} > INT19
    .int20 : {} > INT20
    .int21 : {} > INT21
    .int22 : {} > INT22
    .int23 : {} > INT23
    .int24 : {} > INT24
    .int25 : {} > INT25
    .int26 : {} > INT26
    .int27 : {} > INT27
    .int28 : {} > INT28
    .int29 : {} > INT29
    .int30 : {} > INT30
    .int31 : {} > INT31
    .int32 : {} > INT32
    .int33 : {} > INT33
    .int34 : {} > INT34
    .int35 : {} > INT35
    .int36 : {} > INT36
    .int37 : {} > INT37
    .int38 : {} > INT38
    .int39 : {} > INT39
    .int40 : {} > INT40
    PORT2 : { * ( .int41 ) } > INT41 type = VECT_INIT
    PORT1 : { * ( .int42 ) } > INT42 type = VECT_INIT
    ADC : { * ( .int43 ) } > INT43 type = VECT_INIT
    USCI_B0 : { * ( .int44 ) } > INT44 type = VECT_INIT
    USCI_A1 : { * ( .int45 ) } > INT45 type = VECT_INIT
    USCI_A0 : { * ( .int46 ) } > INT46 type = VECT_INIT
    WDT : { * ( .int47 ) } > INT47 type = VECT_INIT
    RTC : { * ( .int48 ) } > INT48 type = VECT_INIT
    TIMER3_A1 : { * ( .int49 ) } > INT49 type = VECT_INIT
    TIMER3_A0 : { * ( .int50 ) } > INT50 type = VECT_INIT
    TIMER2_A1 : { * ( .int51 ) } > INT51 type = VECT_INIT
    TIMER2_A0 : { * ( .int52 ) } > INT52 type = VECT_INIT
    TIMER1_A1 : { * ( .int53 ) } > INT53 type = VECT_INIT
    TIMER1_A0 : { * ( .int54 ) } > INT54 type = VECT_INIT
    TIMER0_A1 : { * ( .int55 ) } > INT55 type = VECT_INIT
    TIMER0_A0 : { * ( .int56 ) } > INT56 type = VECT_INIT
    UNMI : { * ( .int57 ) } > INT57 type = VECT_INIT
    SYSNMI : { * ( .int58 ) } > INT58 type = VECT_INIT
    .reset : {} > RESET /* MSP430 Reset vector */

    .jtagsignature : {} > 0x1830 /* MSP430 vector table copyed to info memory */
    .bslsignature : {} > 0x1834
    PORT2 : {} > 0x1838
    PORT1 : {} > 0x183A
    ADC : {} > 0x183C
    USCI_B0 : {} > 0x183E
    USCI_A1 : {} > 0x1840
    USCI_A0 : {} > 0x1842
    WDT : {} > 0x1844
    RTC : {} > 0x1846
    TIMER3_A1 : {} > 0x1848
    TIMER3_A0 : {} > 0x184A
    TIMER2_A1 : {} > 0x184C
    TIMER2_A0 : {} > 0x184E
    TIMER1_A1 : {} > 0x1850
    TIMER1_A0 : {} > 0x1852
    TIMER0_A1 : {} > 0x1854
    TIMER0_A0 : {} > 0x1856
    UNMI : {} > 0x1858
    SYSNMI : {} > 0x185A
    .reset : {} > 0x185C /* MSP43O vector table copied to info memory */

    }

    /****************************************************************************/
    /* Include peripherals memory map */
    /****************************************************************************/

    -l msp430fr2433.cmd

    When we are trying to copy the reset vector information from the INFO memory, it is pointing reset vector address inside the info memory alone. not pointing the 0xFFFE.  

    For the above linker cmd the reset vector address pointing either bootloader code or application, not both.

    Please assist any changes to be done with linker command file or any other suggestions.

    Thanks in advance.

  • Hi,

    Okay understand.

    In this document there are some BSL example code provided in it. You can check the demo app code which the .cmd file has been changed to a different location. You can try with it.

    https://www.ti.com/lit/an/slaa721e/slaa721e.pdf

    https://software-dl.ti.com/msp430/msp430_public_sw/mcu/msp430/MSP430FRBoot/latest/index_FDS.html

    Best regards,

    Cash Hao

**Attention** This is a public forum