Tool/software:
Hello,
Few months ago I had a problem with a blocking code iUSS closed source library n
USS_runAlgorithmsFixedPoint(&gUssSWConfig,&algResultsFixedPoint); which was fixed.
We did not change the code or the peripherals but replaced the package type from MSP430FR5043IRGCT with MSP430FR5043 IPM. Both chips report correctly MSP430FR5043 but the new *IPM shows again the same result using the changed code from the thread above.
Any idea? I would assume that the chips inside the two packaging variants are 100 % identical
Regards
Christian