This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi
I have one question about the register of Msp430Fr6972, the register FRCTL0.
I see that on the file MSP430fr6972.h the register FRCTL0 have not defined
the flags WPROT and AUTO, I'm using code composer studio.
This is a Mistake or is better do not using this 2 flags?
If I enable the Auto is automatic generate a wait state, actually I have 16mhz so I'm using NWAITS_1.
I think is confortable to using the WPROT bit because I have using for the Fram the protecion MPU section
but for the Info memory protection I think is this flag that must be used, I would like to using the Info like eeprom,
so protect during nomal operation I will set the Bit Wprot and when I want to write the info memory I will clear the Wprot bit.
The bit Wprot do not have any effect on the MPU segmentation protection memory Right ? the MPU have priority on the meory protection right ?
so when the WPROT is clear all protect memory segmentatio is protect of course, right?
Regards
Luigi
Hey Luigi,
I'm confirming what Bruce said. The FR6972 has the FRCTL, not the FRCTL_A. So those bits are not available.
Thanks,
JD
**Attention** This is a public forum