Part Number: MSP430FR6047
Other Parts Discussed in Thread: TDC7200EVM, TDC7200, MSP-EXP430F5529LP, UNIFLASH,
Tool/software:
Hi Ti Family,
I am trying to update the firmware for my MSP430 LaunchPad (used with the TDC7200EVM) using the TDC7200 GUI, but I’m encountering an issue.
Issue Description:
- The Update Firmware button in the GUI is grayed out and inaccessible.
- The GUI displays "No Device Connected."
- In Device Manager, the MSP430 LaunchPad shows up as:
- MSP Application UART1
- MSP Debug Interface
- USB Serial Device
I’ve tried the following steps without success:
- Reinstalled Drivers: Reinstalled the TDC7200 GUI and ensured the drivers were installed. The LaunchPad is recognized in Device Manager but not by the GUI.
- Entered BSL Mode:
- Disconnected the USB cable.
- Pressed and held the BSL button (or RESET button).
- Reconnected the USB cable while holding the button, then released it.
- The GUI still does not detect the device.
- Checked Firmware Path: Verified that the firmware files are located in
C:\Program Files (x86)\Texas Instruments\TDC7200EVM\Firmware.
Setup Details:
- MSP430 LaunchPad connected to TDC7200EVM via J1 and J2 headers.
- Windows 10 (64-bit).
- USB cable supports data and power transfer.
Any help or insights would be greatly appreciated!
Thanks in advance.