Part Number: MSP430F5437
Other Parts Discussed in Thread: REP430F, SN74LVC1T45
Tool/software:
Hello,
My intention is to complement Replicator REP430F with custom code that allows communication and programming replicator with desired image.
My problem is that I cannot bring UART to work. I haven't found any notes that BSL-RX and TX pins cannot be used for user application as UART line.
Currently, I use Replicator430F from slau320 repository as a base code.
Here is my UART code:
#include "Config430.h" // High-level user input
#include "driverlib.h"
#include "debug_log.h"
#ifdef MCLK_18MHZ
#define MCLK_FREQ 18000000 // 18 MHz
#else
#define MCLK_FREQ 12000000 // 12 MHz
#endif
#define UART_BASE USCI_A0_BASE
#define UART_BAUD_RATE 115200
bool is_init_done = 0;
void Debug_UART_Init(void)
{
if (!is_init_done)
{
GPIO_setOutputLowOnPin(GPIO_PORT_P2, GPIO_PIN0);
// Configure UART pins: P3.4 = UCA0TXD, P3.5 = UCA0RXD
GPIO_setAsPeripheralModuleFunctionInputPin(
GPIO_PORT_P3,
GPIO_PIN4 | GPIO_PIN5
);
// Calculate baud rate settings
uint32_t clockSource = MCLK_FREQ;
uint32_t baudRate = UART_BAUD_RATE;
uint32_t n = clockSource / baudRate; // ~ 104.1667
uint32_t brdiv = n / 16; // = 6
uint32_t remainder = n - (brdiv * 16); // ~ 8.1667
uint32_t firstMod = (uint32_t)( ( (float)remainder / 16.0 ) * 16 + 0.5 ); // ~ 8
uint32_t secondMod = 0; // Approximation for minimal setup
// Initialize UART configuration structure
USCI_A_UART_initParam uartParams = {
.selectClockSource = USCI_A_UART_CLOCKSOURCE_SMCLK,
.clockPrescalar = 6, // brdiv,
.firstModReg = 8, // firstMod,
.secondModReg = 0, // secondMod,
.parity = USCI_A_UART_NO_PARITY,
.msborLsbFirst = USCI_A_UART_LSB_FIRST,
.numberofStopBits = USCI_A_UART_ONE_STOP_BIT,
.uartMode = USCI_A_UART_MODE,
.overSampling = USCI_A_UART_OVERSAMPLING_BAUDRATE_GENERATION
};
// Initialize UART module
if (STATUS_FAIL == USCI_A_UART_init(UART_BASE, &uartParams)) {
// Initialization failed
while(1);
}
// Enable UART module
USCI_A_UART_enable(UART_BASE);
// Clear any pending interrupts
USCI_A_UART_clearInterrupt(UART_BASE, USCI_A_UART_RECEIVE_INTERRUPT);
is_init_done = 1;
}
}
void Debug_UART_Log(const char* message)
{
while(*message)
{
USCI_A_UART_transmitData(UART_BASE, *message++);
}
}This code is added after general MCU initialization from file Replicator430.c
void runProgramm(void)
{
//! \brief Data pointer
word p;
//! \brief Buffer, used for memory read with ReadMemQuick()
word ReadArray[0x40];
/*------------------------------------------------------------------------------------------------------*/
/* 1. | Initialize host MSP430 (on Replicator board) & target board */
/*------------------------------------------------------------------------------------------------------*/
InitController(); // Initialize the host MSP430F5437
ShowStatus(STATUS_ACTIVE, 0); // Switch both LEDs on to indicate operation.
Debug_UART_Init();
Debug_UART_Log(test_msg);
What I tried:
1. I verified that clock works and set to 12 Mhz(choose in config file), by enabling test through the pin and checking with logic analyzer.
2. I tried to use internal UART loop back and it works, I see register values change when I try to TX, RX register is populated with same value, if I enable interrupts, they also trigger.
3. I set level shifter SN74LVC1T45 (REP430F schematic), to output process signal B->A direction P2.0 LOW output. see document REP430F user guide for schematic.
4. I connected FTDI serial cable to check output and I see nothing. I cannot logic analyzer and it also doesn't register any signaling.
Any help would be appreciated!