I am using F2350 µC.
Power for the µC will come from CR2032 battery. To monitor this battery’s voltage level, I can use internal reference voltages (1.8V or 2.5V) and some firmware. No additional component is needed. Correct?
There is another battery in this system. The starting voltage for that battery will be 1.5V (single AA cell). How can this voltage be monitored? Any reference design.
Can this battery be connected to CA0 (pin 15) and internal voltage reference be used also?
Thanks,