This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Benny,
i think the main difference is for 1) you can't do debugging anymore, because the output format is not suitable for the C-SPY IAR debugger. I would recommend you to use the option 2), since then you can still do debugging with the "main output" which is C-SPY compatible.
Hi Benny,
i made a small test, and you are right, using the optino 2) it seems the code is a little bit bigger. Although i am not 100% sure about his, i think the difference is that in option 2), you have to basically choose the "Debug Information for C-SPY" under "Output" tab, and then click the "Allow C-SPY specific extra output file" check box. Therefore i think in option 2) the code will also include some IAR C-SPY specific debugging information and thus makes the code bigger.
However i believe both option should work the same.
**Attention** This is a public forum