This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Eric,
I dont know weather MSP430F2274 has a ready made I2C library, but if u r talking about one to make for yourself, TI examples are best one to start.I have made my library for MSP430g2553 have a look here and go!
#include "I2CMaster.h"
volatile uint16_t I2CNumBytes;
volatile uint16_t Ack;
volatile uint8_t *I2CRxBuffer, *I2CTxBuffer;
volatile uint16_t I2CStop;
void I2CInit( void )
{
P1SEL |= BIT6 + BIT7; // Assign I2C pins to USCI_B0
P1SEL2|= BIT6 + BIT7;
// P1OUT |= BIT6 + BIT7; // We can enable internal pull-ups
// P1REN |= BIT6 + BIT7;
UCB0CTL1 |= UCSWRST; // Enable SW reset
UCB0CTL0 = UCMST + UCMODE_3 + UCSYNC; // 7-bit addressing, single-master environment, I2C Master, synchronous mode
UCB0CTL1 = UCSSEL_2 + UCSWRST; // Use SMCLK, keep SW reset
UCB0BR0 = I2C_400KHZ; // fSCL = SMCLK/UCB0BR1
UCB0BR1 = 0;
UCB0I2CIE = UCNACKIE; // Enable not-acknowledge interrupt
UCB0CTL1 &= ~UCSWRST; // Clear SW reset, resume operation
IE2 |= UCB0TXIE + UCB0RXIE; // Enable TX&RX interrupts
}
uint16_t I2CWrite( uint8_t sladdr , uint8_t *data , uint16_t n )
{
//
Ack = 1; // Return value
//
I2CTxBuffer = data; // TX array start address
I2CNumBytes = n; // Update counter
UCB0I2CSA = sladdr; // Slave address (Right justified, bits6-0)
//
UCB0CTL1 |= UCTR + UCTXSTT; // Send I2C start condition, I2C TX mode
LPM0; // Enter LPM0
//
while( UCB0CTL1 & UCTXSTP ); // I2C stop condition sent?
//
return Ack;
}
uint16_t I2CRead( uint8_t sladdr , uint8_t *data , uint16_t n )
{
//
Ack = 1; // Return value
//
I2CRxBuffer = data; // Start of RX buffer
UCB0I2CSA = sladdr; // Slave address (Right justified, bits6-0)
//
UCB0CTL1 &= ~UCTR; // I2C RX mode
//
if( n == 1 )
{
I2CNumBytes = 0; // Update counter
//
__disable_interrupt();
UCB0CTL1 |= UCTXSTT; // Send I2C start condition, I2C RX mode
while( UCB0CTL1 & UCTXSTT ); // I2C start condition sent?
UCB0CTL1 |= UCTXSTP; // Send I2C stop condition
I2CStop = 1; // I2C stop condition sent
__enable_interrupt();
}
else if( n > 1 )
{
I2CStop = 0; // I2C stop condition not sent yet
I2CNumBytes = n - 2; // Update counter
UCB0CTL1 |= UCTXSTT; // Send I2C start condition
}
LPM0; // Enter LPM0
//
while( UCB0CTL1 & UCTXSTP ); // I2C stop condition sent?
//
return Ack;
}
#ifdef I2C_PING
uint16_t I2CPing( uint8_t sladdr )
{
//
UCB0I2CSA = sladdr; // Slave address (Right justified, bits6-0)
//
__disable_interrupt();
UCB0CTL1 |= UCTR + UCTXSTT + UCTXSTP; // I2C start condition, I2C TX mode, I2C stop condition
while( UCB0CTL1 & UCTXSTP ); // I2C stop condition sent?
Ack = !(UCB0STAT & UCNACKIFG); // I2C start condition akd'd or not?
__enable_interrupt();
//
return Ack;
}
#endif /* !I2C_PING */
#pragma vector = USCIAB0TX_VECTOR
__interrupt void USCIAB0TX_ISR(void)
{
if( IFG2 & UCB0RXIFG ) // RX mode
{
if( I2CNumBytes == 0 )
{
// I2CStop is used just to make sure that we leave LPM0 at the right time and not
// before
if( I2CStop )
{
_low_power_mode_off_on_exit( ); // Exit LPM0
}
else
{
UCB0CTL1 |= UCTXSTP; // I2C stop condition
I2CStop = 1; // I2C stop condition sent
}
}
else
{
I2CNumBytes--; // Decrement counter
}
*I2CRxBuffer++ = UCB0RXBUF; // Read RX data. This automatically clears UCB0RXIFG
}
else // TX mode
{
if( I2CNumBytes ) // Check counter
{
UCB0TXBUF = *I2CTxBuffer++; // Load TX buffer. This automatically clears UCB0TXIFG
I2CNumBytes--; // Decrement counter
}
else
{
UCB0CTL1 |= UCTXSTP; // I2C stop condition
IFG2 &= ~UCB0TXIFG; // Clear USCI_B0 TX int flag
_low_power_mode_off_on_exit( ); // Exit LPM0
}
}
}
#pragma vector = USCIAB0RX_VECTOR
__interrupt void USCIAB0RX_ISR(void)
{
// Not-acknowledge interrupt. This flag is set when an acknowledge is expected
// but is not received. UCNACKIFG is automatically cleared when a START condition
// is received.
if( UCB0STAT & UCNACKIFG )
{
UCB0CTL1 |= UCTXSTP; // I2C stop condition
Ack = 0; // Return value
UCB0STAT &= ~UCNACKIFG; // Clear interrupt flag
}
// Arbitration-lost. When UCALIFG is set the UCMST bit is cleared and the I2C
// controller becomes a slave. This can only happen in a multimaster environment
// Start condition detected interrupt. UCSTTIFG only used in slave mode.
// Stop condition detected interrupt. UCSTPIFG only used in slave mode.
_low_power_mode_off_on_exit( ); // Exit LPM0
}
Hi Sri-sri,
Thanks a lot for your piece of code. I have implemented it and it runs fine.
I would like to ask you some additional questions:
The Delay function source code is as follows:
void Delay(unsigned int Count)
{
TACCTL0 &= ~CCIFG; // Reset CCIFG Interrupt Flag
TACCTL0 = CCIE; // TACCR0 interrupt enabled
TACTL = TASSEL_1 + MC_1; // Timer A select, clock source ACLK, count up to TACCR0, activate Interrupt Request
TACCR0 = Count; // Clock Count/32'768 s, load Capture Compare of Timer A
__bis_SR_register(LPM3_bits + GIE); // Enter LPM3, enable interrupts, only TIMERA Interrupt available
}
// Timer A0 interrupt service routine
#pragma vector=TIMERA0_VECTOR
__interrupt void Timer_A(void)
{
TACCR0 = 0; // Stop TIMERA
TACCTL0 &= ~CCIE; // TACCR0 interrupt disabled
__bic_SR_register_on_exit(LPM3_bits /*+ GIE*/); // Exit LPM3: GIE commented because of an interrupt
// conflict with I2C functions (EMe 16.10.2012)
}
The clock system configuration is as follows:
WDTCTL = WDTPW + WDTHOLD; // Stop WDT
BCSCTL3 |= (XCAP0 + XCAP1); // Set ACLK Capacity to 12.5 pF
BCSCTL1 = CALBC1_1MHZ; // DCO = 1MHz
DCOCTL = CALDCO_1MHZ;
Again, thanks for all!
Best regards,
Eric.
AS I see the code, stop isn't "monitored". The only condition monitored is the NACK.Eric MEURVILLE said:Why it is necessary to monitor the stop condition:
It is rather uncommon that you send or receive more data later while keeping the I2C busy. I2C is a transaction-based protocol, not a connection-based one. A transaction is initiated and finished. You can compare it with UDP, not with TCP.Eric MEURVILLE said:suppress the generation if I2C stop conditions both in I2CRead and I2CWrite functions when I want to leave the communication channel open for further transactions?
It's possible that the I2C functions require GIE set but don't set it themselves.Eric MEURVILLE said:noticed a conflict when GIE are set when exiting LPM3. Do you know why?
Strange. The 'original' code uses 'I2C_400kHz' constant. Well, difficult on 1Mhz SMCLK, as 2.5 isn't a valid value for BR0. :)Eric MEURVILLE said:When I change UCB0BR0 from 10 to 5, I do not observe a change in SCL frequency
Hi Eric,
Jens had explained everything and it sound cool,, Just a small addition to it, it you want to know much about the code and its process(lets say I2C coz I got much of the code form TI itself,)
1.Remove one of the Pull up the pul up resistor and try to debug the code(step by step) code will halt in while() //stop condition sent after LPM0.
2. Try sending wrong address of your EEPROM insted of 0x50 and c
you learn much from mistakes and quick research gives u a lot more Idea.
As regards to UCB0BR0 you said a change from 10 to 5..y ? what is your desired frequency ?
ex: if you want a I2C communication of 100khz ucb0bro == 160. i.e, fre = fmclk/ucb0br0 16Mhz/160 = 100K
Regards,
sri.
Hi Jens-Michael,
Thanks a lot for your help. Everything is clear now. With regards to the SCL frequency, the issue comes form the length of the line between the master and the slave. So, adapting the pull up value is the good way.
Thanks again and Best regards,
Eric.
Hi All,
We are considering porting this code that works pretty well onto an MSP430FR5739. Did someone already do that?
Thanks and regards,
Eric.
sri-sri said:Hi Eric,
I dont know weather MSP430F2274 has a ready made I2C library, but if u r talking about one to make for yourself, TI examples are best one to start.I have made my library for MSP430g2553 have a look here and go!
#include "I2CMaster.h"
volatile uint16_t I2CNumBytes;
volatile uint16_t Ack;
volatile uint8_t *I2CRxBuffer, *I2CTxBuffer;
volatile uint16_t I2CStop;
void I2CInit( void )
{
P1SEL |= BIT6 + BIT7; // Assign I2C pins to USCI_B0
P1SEL2|= BIT6 + BIT7;
// P1OUT |= BIT6 + BIT7; // We can enable internal pull-ups
// P1REN |= BIT6 + BIT7;
UCB0CTL1 |= UCSWRST; // Enable SW reset
UCB0CTL0 = UCMST + UCMODE_3 + UCSYNC; // 7-bit addressing, single-master environment, I2C Master, synchronous mode
UCB0CTL1 = UCSSEL_2 + UCSWRST; // Use SMCLK, keep SW reset
UCB0BR0 = I2C_400KHZ; // fSCL = SMCLK/UCB0BR1
UCB0BR1 = 0;
UCB0I2CIE = UCNACKIE; // Enable not-acknowledge interrupt
UCB0CTL1 &= ~UCSWRST; // Clear SW reset, resume operation
IE2 |= UCB0TXIE + UCB0RXIE; // Enable TX&RX interrupts
}
uint16_t I2CWrite( uint8_t sladdr , uint8_t *data , uint16_t n )
{
//
Ack = 1; // Return value
//
I2CTxBuffer = data; // TX array start address
I2CNumBytes = n; // Update counter
UCB0I2CSA = sladdr; // Slave address (Right justified, bits6-0)
//
UCB0CTL1 |= UCTR + UCTXSTT; // Send I2C start condition, I2C TX mode
LPM0; // Enter LPM0
//
while( UCB0CTL1 & UCTXSTP ); // I2C stop condition sent?
//
return Ack;
}
uint16_t I2CRead( uint8_t sladdr , uint8_t *data , uint16_t n )
{
//
Ack = 1; // Return value
//
I2CRxBuffer = data; // Start of RX buffer
UCB0I2CSA = sladdr; // Slave address (Right justified, bits6-0)
//
UCB0CTL1 &= ~UCTR; // I2C RX mode
//
if( n == 1 )
{
I2CNumBytes = 0; // Update counter
//
__disable_interrupt();
UCB0CTL1 |= UCTXSTT; // Send I2C start condition, I2C RX mode
while( UCB0CTL1 & UCTXSTT ); // I2C start condition sent?
UCB0CTL1 |= UCTXSTP; // Send I2C stop condition
I2CStop = 1; // I2C stop condition sent
__enable_interrupt();
}
else if( n > 1 )
{
I2CStop = 0; // I2C stop condition not sent yet
I2CNumBytes = n - 2; // Update counter
UCB0CTL1 |= UCTXSTT; // Send I2C start condition
}
LPM0; // Enter LPM0
//
while( UCB0CTL1 & UCTXSTP ); // I2C stop condition sent?
//
return Ack;
}
#ifdef I2C_PING
uint16_t I2CPing( uint8_t sladdr )
{
//
UCB0I2CSA = sladdr; // Slave address (Right justified, bits6-0)
//
__disable_interrupt();
UCB0CTL1 |= UCTR + UCTXSTT + UCTXSTP; // I2C start condition, I2C TX mode, I2C stop condition
while( UCB0CTL1 & UCTXSTP ); // I2C stop condition sent?
Ack = !(UCB0STAT & UCNACKIFG); // I2C start condition akd'd or not?
__enable_interrupt();
//
return Ack;
}
#endif /* !I2C_PING */
#pragma vector = USCIAB0TX_VECTOR
__interrupt void USCIAB0TX_ISR(void)
{
if( IFG2 & UCB0RXIFG ) // RX mode
{
if( I2CNumBytes == 0 )
{
// I2CStop is used just to make sure that we leave LPM0 at the right time and not
// before
if( I2CStop )
{
_low_power_mode_off_on_exit( ); // Exit LPM0
}
else
{
UCB0CTL1 |= UCTXSTP; // I2C stop condition
I2CStop = 1; // I2C stop condition sent
}
}
else
{
I2CNumBytes--; // Decrement counter
}
*I2CRxBuffer++ = UCB0RXBUF; // Read RX data. This automatically clears UCB0RXIFG
}
else // TX mode
{
if( I2CNumBytes ) // Check counter
{
UCB0TXBUF = *I2CTxBuffer++; // Load TX buffer. This automatically clears UCB0TXIFG
I2CNumBytes--; // Decrement counter
}
else
{
UCB0CTL1 |= UCTXSTP; // I2C stop condition
IFG2 &= ~UCB0TXIFG; // Clear USCI_B0 TX int flag
_low_power_mode_off_on_exit( ); // Exit LPM0
}
}
}
#pragma vector = USCIAB0RX_VECTOR
__interrupt void USCIAB0RX_ISR(void)
{
// Not-acknowledge interrupt. This flag is set when an acknowledge is expected
// but is not received. UCNACKIFG is automatically cleared when a START condition
// is received.
if( UCB0STAT & UCNACKIFG )
{
UCB0CTL1 |= UCTXSTP; // I2C stop condition
Ack = 0; // Return value
UCB0STAT &= ~UCNACKIFG; // Clear interrupt flag
}
// Arbitration-lost. When UCALIFG is set the UCMST bit is cleared and the I2C
// controller becomes a slave. This can only happen in a multimaster environment
// Start condition detected interrupt. UCSTTIFG only used in slave mode.
// Stop condition detected interrupt. UCSTPIFG only used in slave mode.
_low_power_mode_off_on_exit( ); // Exit LPM0
}
Hi
I am working MSP430FR5739 by TI. i am tryng to bring up I2C interface between MSP430 and external acceleromer. Is there any api like I2C write in MSP430FR5739 to configure external accelerometer from the master.. Please help me to solve this issue..
Thanks and regards
Ck
**Attention** This is a public forum