Other Parts Discussed in Thread: MSP430FR5725, MSP-EXP430FR5739, MSP430G2553, MSP430G2231
Hi,
I'm trying to send commands to my BSL using the MSP430 Lauchpad and BSL_Scripter. I did what is explained in the application note SLAA535A.
I think that my MSP430 is successfully entering in the BSL, but when I try to send any command with the BSL_Scripter I always get the error "0x54 - Packet size exceeds buffer. The packet size given is too big for the RX buffer"
Here is what I try to send:
MODE 5xx COM6
VERBOSE
DELAY 1000
TX_BSL_VERSION
The output:
------------------------------------------
BSL Scripting application 1.06
The local time is: 08:45 on 16.10.2012
------------------------------------------
Initializing, Mode: 5xx COM: COM6 DONE
Verbose mode on
Waiting 1000 milliseconds DONE
-------------------------------------------------
[80] [01] [00] [19] [e8] [62] {54}
-------------------------------------------------
BSL Version: ERROR
Whatever I try to send I get errors.
I attached the serial frame grabbed with my logic analyser.
Any suggestions ?
Thanks
Nicolas