Hello. I was wondering if it is possible to control a pin via the PWM functionality of a timer without setting PxSEL |= BITn? I have a pin that I would like to control via PWM, but it is not connected to a timer module, like TAx.n. I am using the MSP430FR5725. The pin description is "PJ.0/TDO/TB0OUTH/SMCLK/CD6".