I have been used ADC12 of MSP430F4619.now I'm trying to learn msp430F6746 for my next project, I don't know how to use SD24_B, is it similar to ADC12 ? for example, for ADC, it need a REF,like 1.5V, I have to adjust input signal to 1.5V when it is full range. How about SD24_B ? I don not want to know the detail of princple, but I want to know how to use it, could you give me some link of sample code and application? in my appliation, I will measure Pressure and Temperature, the input is 0-10mv signal. before I use OP to adjust signal to 0-1.5V, then add it onto ADC12, how about now if I use SD24_B in the msp430F6746 ?