When i doing the FW upgrade in MSP430F5308 base on the way of slaa535, it works well when i use the launchpad as the bridge between PC side and the target MSP430F5308, and the normal feedback from MSP430 will be message of "{80} {02} {00} {3b} {00} {60} {c4}"
But when i replace the lunchpad to my real system main chip(ARM base MPU) doing the FW upgrade, it has a big chance to be fail, and the feedback message from MSP430 will be "{80} {02} {00} {3b} {00} {60} {23}"
i check the baud rate on osciallscope, it is exact 9600bit/s, and the byte to byte interval is approx 1.3ms,
is there any timing issue cause the failure or something i miss?