This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

430.hex how to use stand alone

Expert 2355 points

Hi,

Now I need to convert from *.d43 file to *.txt or *.hex.

hex430.exe can convert it.

But There is no procedure to use standalone without CCS.

C:\ti\ccsv5\tools\compiler\msp430_4.1.5\bin

Pls tell me how to use hex430.exe in stand alone.

best regards

  • I do not know CCS. But IAR Linker has the option to generate the object file in various formats. The IAR Debugger also has the option to save or restore  the Flash image to or from a file in various formats.

    420Flasher and most "Programmer" can also save or retrieve Flash image to or from a file in various formats.

**Attention** This is a public forum