This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'd like to implement a stand-alone programmer in production for the MSP432P401R like I have for the MSP430 using the MSP-FET430UIF and Elpotronic FetProLite. The MSP432P401R has a small footprint JTAG connector (2x5 @ J102) instead of the 0.1 center 14 pin standard JTAG.
Is there a "mini" JTAG cable available for the MSP-FET430UIF that will work with the MSP432P401R?
Will MSP430 Flasher work with the MSP432P401R?
Is the MSP-FET required to work with the MSP432P401R and is a "mini" JTAG cable available?
Will Elpotronic FetProLite work with the MSP432P401R?
I'm basically looking for a hardware / software utility solution to stand-alone program the MSP432P401R.
Thanks.
s.chancey@heathus.com
Thorsten Stauber said:But the adapter needs to be purchased of course.
:) Sure!
That is great! Was thinking I would maybe need to get another (newer) one then. But if it is done with a firmware update, I'm looking forward to it - great news!
Dennis
**Attention** This is a public forum