This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I have several boards with 5529 MCUs on them. I need to change the BSL on them. Are there instructions on how to do this and what tools are required? Note, these boards are not powered by USB but we do use the USB interface to perform firmware updates on the main code? Thanks.
Using SBW / JTAG, BSL area can be flashed like main flash, just need to be BSL unlocked first. It is not important is it board powered by USB or not. Probably it can be done by all tools, example with my flasher...
D:\msp430>flash -p com21 -f bsl5510.txt -ubsl -ebsl -w -v
File "bsl5510.txt"
Address: 01000 Words: 1024
2048 bytes
Get Device
# JTID Fuse Device Core Hard Soft LotWafer DieX DieY
0 91 OK 3180 1104 12 12 013BB046 2700 2E00
Unlock BSL
Erase BSL
Write
Size: 2048 bytes Time: 50 ms Speed: 39,2 KB/s
Verify
Size: 2048 bytes Time: 15 ms Speed: 126,9 KB/s
Release Device
Total Time: 219 ms
D:\msp430>
**Attention** This is a public forum