Other Parts Discussed in Thread: ADS1293, MSP430F5529, ENERGIA
Hi there
I would like to ask if anyone knows what is the hardware connection that I need and the software to erase the flash memory in the MSP430 ?
I have An ADS1293 Evaluation board with the MSP430F5529IPN as the microcontroller which is used to read/write registers of the ADS1293, what I want to do is to erase the flash memory of the MSP430 as was suggested to me to make my evaluation board communicate with the Arduino uno device through the SPI port to read the data using the Arduino software
so let me know if you have anything useful
Thanks