This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello every one,
i am working the TSS721A tranceiver with the MSP430 processor to make a m-bus slave.
i used it as marked in the datasheet to develop this circuit below,
but when i send data on the bus from a master i have nothing on the pin TX.
can anyone help me please to find out what could be the problem with this circuit !
note : the processor is powered independently and not using the 3.3Vprovided by the tss721A, and the Mbus_SL_TX and Mbus_SL_RX is connected to the MSP430 UART.
thanks for your help.
I don't think there is a problem wiht TXI connected to RX. The optocoupler does an inversion, so things seem to be connected right.
Taking as given that the physical connection is correct, there might be a software setup problem. Did you program the ports for USART module usage? (else they are plain GPIO pins)
A look at your code yould be enlightening.
Also, there is no 'the MSP430 processor', but a family of ~270 different processors divided into several sub-families. A hint which one you use would be a great help too.
**Attention** This is a public forum