Other Parts Discussed in Thread: MSP430G2233
My application need one Capacitive Touch buttom, three PWM signal, one I2C, which MSP430Gxx series MCU could be selected.
Does MSP430G2233 could achieve these function.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP430G2233
My application need one Capacitive Touch buttom, three PWM signal, one I2C, which MSP430Gxx series MCU could be selected.
Does MSP430G2233 could achieve these function.
Because you do not need ADC, if G2233 works for you, so would G2203. For that mater, any of the other 6 chips included in the data-sheet of G2233 would work for you too.
I think it might be difficult to do Capacitive Touch sensing and 3 PWM at the same time with any one of those 7 chip. The Timer0_A3 can only generate 1 PWM and the Timer1_A3 can generate 2 PWM. This means you need to use both Timers to have 3 PWM. Capacitive Touch sensing will need Timer0_A3 CC2, But it Timer0_A3 is in count up to CC0 mode due to PWM, can you still use CC2 for Capacitive Touch sensing?
old_cow_yellow said:Timer0_A3 is in count up to CC0 mode due to PWM
To get PWM, you can use continuous mode (count to timer overflow), thus you get CCR0 for PWM output too. That's why I asked question about PWM frequency. 244Hz (16MHz/65536) is more than enough for LED brightness control for instance
**Attention** This is a public forum