Hi all,
I have used the parametric search tool but am not having any luck finding what I'm looking for. Rather than moving on I decided to ask here if someone might have a suggestion.
I have a need for a low power microcontroller with an 8-10bit ADC (one channel is enough) that runs at a clock rate of 9kHz or less (no clock on the chip can be higher than this).
The rest of the parameters I can sort through if someone can point me in the right direction, but here are a few
VDD 3V
Iquiescent < 2mA
at least 15 I/O
Thanks,
sne