Other Parts Discussed in Thread: MSP430-FLASHER, MSP-FLASHER, MSP430G2553, MSP-EXP430FR5969, MSP430FR5969
I'm using the command line MSP430 flasher, v 1.3.3 I believe, in XP, and when I read the current contents of a device to an Intel hex file, the flasher writes in 32-byte lines, so they start ":20". Is there a switch or other way to persuade the flasher to use 16-byte lines? Of course I could convert later, but would just rather have it the way I want it to begin with. If not in 1.3.3, is there a later version that provides this option?