Other Parts Discussed in Thread: MSP430FR6989
Hello
I am using the LaunchPad Eval Kit with the MSP430FR69891 uP.
I want to use the SPI Interface USCIA0 in slave mode, 4 pin mode active high, with clock phase flag UCCKPH=1 enabled
I have the UCA0IE set and also GIE is set. On the Logic Analyzer i can see that the UCA0STE pin goes high, the clock is working the data (SIMO) is correct but the interrupt gets not activated.
I could observe that if i don't set the UCCKPH (UCCKPH=0) the interrupts are working and also if i do the configuration of the SPI interface with the UCSWRST=0 (which is incorrect) it is also working,
I am using CCS 7 with GNU compiler (GNU v6.2.1.16 DOMNIUM Technologies Limited)
Here my configuration:
void initializeUca0Spi(void)
{
// Configure USCI_A0 for SPI operation
UCA0CTLW0 = UCSWRST; // **Put state machine in reset**
#if (RX_MODE == 1)
UCA0CTLW0 |= UCSYNC | UCMSB | UCCKPH | UCMODE_1;
#else
UCA0CTLW0 |= UCSYNC | UCMSB | UCCKPH;
#endif
UCA0CTLW0 &= ~UCSWRST;
#if (RX_MODE == 1)
UCA0IE |= UCRXIE;
__no_operation();
#endif
}
any ideas?
Thanks in advance