Dear Brian,
Thank you, for your inputs and support to fix this issue.
Please, help me in updating the firmware by using binary file project_name.out.
currently we are following method to update the firmware.
Tools used: Code composer studio V5
Programmer & Debugger used : MSP-FET430UIF ( MSP430 USB - debug Interface).
steps are as follows.
- set the project configuration to Release - MSP430F5438A EXP[Active] in workspace.
- Build All ( Projecct --> Build- All).
- Debug ( Run -- Debug).
I want to use only binary file project_name.out to update the firmware in all devices. Please clarify following ASAP.
- Methods or steps need to be followed to update the firmware using only binary file(project_name.out).
- Is there any way to update the firmware OTA( Over the air )?.
Thanks and Regards,
Bhairu