This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5529: msp430f5529 keypad interfacing

Part Number: MSP430F5529


Hello everyone,

I want to interface keypad 4x4 matrix with msp430f5529. The pins which I need to interface,is not available in the board.

As I have gone through the code I understood that pin 5.7,5.6 ,4.7  and pins from 7.4-7.7 are needed but those are not visible in the headers.

And also pin 2.1 which I need  it is a switch,so i can't work with it.

Q. So can you tell me how can I execute this program? I have attached the file below.Interfacing-Keypad-with-MSP430F5529.pdf

**Attention** This is a public forum