Hi guys,
I was using my MSP-FET430UIF to program a custom PCB with a MSP430F5529 and everything was going fine when suddenly I got the following error:
Error initializing emulator: The voltage 1209 value is not correct/allowed for the USB FET.
I did a little bit of research about the issue and none of the answers I found apply to my situation. I didn't change anything to the supply voltage and I don't think I made any bad manipulation that could cause this problem. In fact I was debugging a piece of software for the last 2+ hours and there was no problems programming my device then this happened seemingly out of nowhere... I tried with another board and got the same error, is it possible that the usb debug interface is broken? It would be great if someone has a solution to this.
Regards