Hello,
I need to know how long the device can survive under the following condition:
MSP430G2332 transmits a 2.2V signal on PIN 13 (P2.6) (Configured as Output) to another controller. However, the controller is not powered up when it sees this 2.2V signal, and this signal powers the controller through the ESD Diode. This pulls the PIN 13 on MSP down and we see a dip from 2.2V to about 1.5V for about 200us.
This condition occurs 50 times a day approximately. How reliable is the MSP430 when it is subject to
Thanks.