This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F438: Screening and Qualification Tests Information

Part Number: MSP430F438


Hello, my name is Gabriel and I work at TEKEVER, Portugal. 
We are currently using the referred component in a space intended project. 
Given the nature of our application, we are required to qualify every component according to standards.
However if you have already performed any test on any of these components it would be most valuable and time saving for us to have knowledge of those tests, which include, for example:
- Preconditioning + HAST or THB 
- C-SAM inspection
- Thermal Cycling / Shock 
- Lifetest

The test conditions are not important, so if you have done any of these tests or other kinds of tests that may comply to any MIL-PRF or STD, it would be most helpful in our qualification process.

Keep in mind that we are aware that some components may not be specific for space applications, however the mission in which these components will be part of, is going to provide a controlled temperature and radiation environment, thus the use of commercial components being allowed.

Thank you and best regards.

  • Hi  Gabriel,

    yes it's part of standard qualification find details below:

                                                                                                                      
                                                        Reliability Test Results
                              
                                                                         
                                                                                                    Sample Size/Results
                         Test Type
                                                                Conditions/Duration                       Lot#1
            
                  **Life Test, 150C                        300 Hours                                  116/0
                  **Thermal Shock,  -65/150C        1000 Cycles                               77/0
                         ESD                                HBM: 4000V                                 3/0
                                                                   HBM: 2000V                              3/0
                                                                   HBM: 1500V                              3/0
                                                                   HBM: 1000V                              3/0
                                                                   HBM: 500V                                3/0
                                                                    MM: 200V                                 3/0
                                                                    MM: 100V                                 3/0
                                                                   CDM: 750V                                3/0
                                                                   CDM: 500V                                3/0
                          Latch-Up                            250mA                                       5/0


    Preconditioning Information:
     ** Preconditioning sequence: JEDEC Level 3 @ 235C


  • Thank you! That's exactly what I was looking for.

    Best regards

**Attention** This is a public forum