This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432P401R: Replacing the XMSP432 of the Black launchpad with MSP432 Production Silicon.

Part Number: MSP432P401R

Hi Everyone,

Just want to ask if I will be going to replace the original MCU placed on the MSP432 Black launchpad

with the production type MSP432P401R, instead of using the original XMSP432P401R.

Will this affect the programming performance of the built in XDS110 on the board itself?

I want to do this because of the issue last time that the XMSP version has an errata on ADC14.

In which, this causes the jumping reading even if filters were supplied and using a good LDO to power it on.

Please advise. 

Thank you,

Leo 

  • Leo,
    Yes, you can replace the XMS silicon with the production type. I have not tried this with the MSP432P401R but with the MSP432P4111 and I have not had any issues with the built in xds110.

    Chris
  • Hi Mr. Chris,

    Thanks. This answers my question.
    At first, I want to buy an MSP432 Red Launchpad.
    And I notice TI released the chip itself to the distributors for the IC purchase.

    Best Regards,
    Leo B. Pestañas

**Attention** This is a public forum